Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
software:linux:docs:iio:iio [30 May 2012 13:36]
mhennerich [IIO Ring Buffer]
software:linux:docs:iio:iio [23 Feb 2017 13:26]
larsc Fix typo
Line 4: Line 4:
 ===== IIO Overview ===== ===== IIO Overview =====
  
-  * The Industrial I/O subsystem is intended to provide support for devices that in some sense are analog to digital or digital to analog ​convertors ​(ADCs, DACs).+  * The Industrial I/O subsystem is intended to provide support for devices that in some sense are analog to digital or digital to analog ​converters ​(ADCs, DACs).
   * Devices that fall into this category are:   * Devices that fall into this category are:
     * ADCs     * ADCs
Line 44: Line 44:
     * These are similar to input in that they provide a route to user space for hardware triggered events. Such events include threshold detectors, free-fall detectors and more complex action detection. ​ The events themselves are currently very simple with merely an event code and a timestamp. ​ Any data associated with the event must be accessed via polling.     * These are similar to input in that they provide a route to user space for hardware triggered events. Such events include threshold detectors, free-fall detectors and more complex action detection. ​ The events themselves are currently very simple with merely an event code and a timestamp. ​ Any data associated with the event must be accessed via polling.
  
-<note>+<WRAP round help>
 A given device may have one or more event channel. ​ These events are turned on or off (if possible) via sysfs interfaces. A given device may have one or more event channel. ​ These events are turned on or off (if possible) via sysfs interfaces.
-</note>+</WRAP>
  
   * Hardware ring buffer support   * Hardware ring buffer support
software/linux/docs/iio/iio.txt · Last modified: 23 Feb 2017 13:26 by larsc