This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
software:linux:docs:iio:iio [23 Feb 2017 13:26] – Fix typo Lars-Peter Clausen | software:linux:docs:iio:iio [05 Jun 2020 17:03] (current) – [IIO Overview] Grammar changes Iulia Moldovan | ||
---|---|---|---|
Line 22: | Line 22: | ||
* The overall aim is to fill the gap between the somewhat similar hwmon and input subsystems. | * The overall aim is to fill the gap between the somewhat similar hwmon and input subsystems. | ||
* Hwmon is very much directed at low sample rate sensors used in applications such as fan speed control and temperature measurement. | * Hwmon is very much directed at low sample rate sensors used in applications such as fan speed control and temperature measurement. | ||
- | * Input is, as it' | + | * The input is (as its name suggests) focused on human interaction input devices: |
* Keyboard | * Keyboard | ||
* Mouse | * Mouse | ||
Line 28: | Line 28: | ||
* Joystick | * Joystick | ||
- | * In some cases there is considerable overlap between these and IIO. | + | * In some cases, there is considerable overlap between these and IIO. |
* A typical device falling into the IIO category would be connected via SPI or I2C. | * A typical device falling into the IIO category would be connected via SPI or I2C. |