Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Last revision Both sides next revision
resources:tools-software:uc-drivers:renesas:adxrs453 [12 Nov 2012 12:57]
DNechita Removed applilet3 content / updated drivers.
resources:tools-software:uc-drivers:renesas:adxrs453 [29 May 2013 13:18]
LucianS added RENESAS RL78G14 QUICK START GUIDE and RL78G14 source code downloads
Line 8: Line 8:
 ===== Downloads ===== ===== Downloads =====
  
-<WRAP round download ​30%>+<WRAP round download ​80%>
   * {{:​resources:​tools-software:​uc-drivers:​adxrs453_generic.zip|ADXRS453 Generic Driver}}   * {{:​resources:​tools-software:​uc-drivers:​adxrs453_generic.zip|ADXRS453 Generic Driver}}
   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adxrs453_rl78g13.zip|ADXRS453 RL78G13 Driver}}   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adxrs453_rl78g13.zip|ADXRS453 RL78G13 Driver}}
   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adxrs453_rx62n.zip|ADXRS453 RX62N Driver}}   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adxrs453_rx62n.zip|ADXRS453 RX62N Driver}}
 +  * **ADXRS453 Driver: ​          ** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​drivers/​ADXRS453
 +  * **PmodGYRO2 Demo for RL78G14: ** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​Renesas/​RL78G14/​PmodGYRO2
 +  * **RL78G14 Common Drivers: ​  ** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​Renesas/​RL78G14/​Common
 </​WRAP>​ </​WRAP>​
  
Line 25: Line 28:
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
-A PmodGYRO2 has to be connected to the PMOD1 connector.+A PmodGYRO2 has to be connected to the PMOD1 connector, pins 1 to 6 (see image below).
  
 {{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_gyro2_rl78g13.jpg?​ |}} {{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_gyro2_rl78g13.jpg?​ |}}
  
 ==== Reference Project Overview ==== ==== Reference Project Overview ====
-The reference project reads the 10-Bit Temperature Data and the 16-Bit Rate Data. The values ​are displayed ​on the LCD as degrees Celsius and degrees/sec respectively.+The reference project
 +  * reads the 10-Bit Temperature Data and the 16-Bit Rate Data
 +  * displays the values on the LCD as degrees Celsius and degrees/sec respectively.
  
 {{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_gyro2_rl78g13_screen.jpg?​ |}} {{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_gyro2_rl78g13_screen.jpg?​ |}}
Line 36: Line 41:
 ==== Software Project Tutorial ==== ==== Software Project Tutorial ====
 {{page>​rl78g13_software_tutorial_without_applilet3}} {{page>​rl78g13_software_tutorial_without_applilet3}}
 +
 +====== Renesas RL78G14 Quick Start Guide ======
 +This section contains a description of the steps required to run the ADXRS453 demonstration project on a Renesas RL78G14 platform using the PmodGYRO2.
 +
 +==== Required Hardware ====
 +  * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrl78g14/​index.jsp|Renesas Demo Kit for RL78G14 (Renesas)]]
 +  * [[http://​www.digilentinc.com/​Products/​Detail.cfm?​Prod=PMOD-GYRO2|PmodGYRO2]]
 +
 +==== Required Software ====
 +  * [[http://​www.iar.com/​en/​Products/​IAR-Embedded-Workbench/​Renesas-RL78/​|IAR Embedded Workbench for Renesas RL78 Kickstart]]
 +  * The ADXRS453 demonstration project for the Renesas RL78G14 platform.
 +
 +<WRAP round info 80%>
 +The ADXRS453 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADXRS453 Driver**, ​ the **PmodGYRO2 Demo for RL78G14** and the **RL78G14 Common Drivers**.
 +
 +All three parts have to be downloaded.
 +</​WRAP>​
 +==== Hardware Setup ====
 +A PmodGYRO2 has to be connected to the PMOD1 connector, pins 1 to 6 (see image below).
 +
 +{{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_gyro2_rl78g14.jpg?​ |}}
 +
 +==== Reference Project Overview ====
 +The reference project:
 +  * reads the 10-Bit Temperature Data and the 16-Bit Rate Data;
 +  * displays the values on the LCD as degrees Celsius and degrees/sec respectively.
 +
 +<WRAP round important 80%>
 +  * If you rotate the Pmod slowly, you will see a smaller value (e.g. 30 Degrees/​Second),​ while rotating the Pmod at a higher speed will result in a higher value (e.g. 300 degrees/​second). Afterwards the device will auto calibrate according to its new position, thus displaying a value close to 0 degrees/​second.
 +</​WRAP>​
 +
 +
 +{{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_gyro2_rl78g14_screen.jpg?​ |}}
 +
 +==== Software Project Tutorial ====
 +{{page>​rl78g14_software_tutorial}}
 +
  
 ====== Renesas RX62N Quick Start Guide ====== ====== Renesas RX62N Quick Start Guide ======
resources/tools-software/uc-drivers/renesas/adxrs453.txt · Last modified: 22 Jul 2019 14:16 by AndreiD1994