This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:adxl345 [12 Nov 2012 10:37] – Removed applilet3 content / updated drivers. Dan Nechita | resources:tools-software:uc-drivers:renesas:adxl345 [24 May 2013 12:54] – Deleted the generic driver. Dragos Bogdan | ||
---|---|---|---|
Line 8: | Line 8: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
- | * {{: | + | |
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **ADXL345 Driver: | ||
+ | * **PmodACL Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: | ||
</ | </ | ||
Line 42: | Line 44: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RL78G14 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the ADXL345 demonstration project on a Renesas RL78G14 platform using the PmodACL. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * PmodACL | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * The ADXL345 demonstration project for the Renesas RL78G14 platform. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The ADXL345 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADXL345 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
+ | ==== Hardware Setup ==== | ||
+ | There are two options: | ||
+ | |||
+ | * The ADXL345 part installed on the Renesas Demonstration Kit (RDK) for RL78G14 can be used. In this case, the I2C protocol has to be chosen with ' | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | * A PmodACL can be connected to the PMOD1 connector. In this case, the SPI protocol has to be chosen with ' | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project: | ||
+ | * reads and displays the data for each axis on LCD; | ||
+ | * it displays also on LCD if the interrupts “Single Tap”, “Double Tap” or “Free-Fall” were activated. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | ==== Software Project Tutorial ==== | ||
+ | {{page> | ||
+ | |||
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== |