Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:tools-software:uc-drivers:renesas:adis16227 [16 Mar 2012 14:23]
dragosb Added the "Software Setup" section and replaced the "Software Project Setup" link.
resources:tools-software:uc-drivers:renesas:adis16227 [16 Nov 2012 16:46] (current)
larsc [Evaluation Boards] fixup eval board link
Line 5: Line 5:
  
 ===== Evaluation Boards ===== ===== Evaluation Boards =====
-  * [[adi>​ADIS16227 | ADIS16227/​PCBZ]]+  * [[adi>EVAL-ADIS16227|ADIS16227/​PCBZ]]
  
 ===== Overview ===== ===== Overview =====
Line 16: Line 16:
 **HW Platform(s):​** **HW Platform(s):​**
   * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrl78g13/​index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]]   * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrl78g13/​index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]]
 +  * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrx62n/​index.jsp|Renesas Demo Kit for RX62N (Renesas)]]
 ===== Driver Description ===== ===== Driver Description =====
 The driver contains two parts: The driver contains two parts:
Line 50: Line 50:
   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_generic.zip|ADIS16227 Generic Driver}}   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_generic.zip|ADIS16227 Generic Driver}}
   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rl78g13.zip|ADIS16227 RL78G13 Driver}}   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rl78g13.zip|ADIS16227 RL78G13 Driver}}
 +  * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rx62n.zip|ADIS16227 RX62N Driver}}
  
 ====== Renesas RL78G13 Quick Start Guide ====== ====== Renesas RL78G13 Quick Start Guide ======
Line 107: Line 108:
 {{page>​rl78g13_software_tutorial}} {{page>​rl78g13_software_tutorial}}
  
 +====== Renesas RX62N Quick Start Guide ======
 +This section contains a description of the steps required to run the ADIS16227 demonstration project on a Renesas RX62N platform.
 +
 +==== Required Hardware ====
 +  * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrx62n/​index.jsp|Renesas Demo Kit for RX62N (Renesas)]]
 +  * [[adi>​ADIS16227 | ADIS16227/​PCBZ (Analog Devices)]]
 +==== Required Software ====
 +  * [[http://​www.renesas.com/​products/​tools/​ide/​ide_hew/​index.jsp|High-performance Embedded Workshop for RX62N family]]
 +  * [[http://​am.renesas.com/​products/​tools/​middleware_and_drivers/​c_driver_gen/​driver_gen_rpdl/​index.jsp|Renesas Peripheral Driver Library for RX62N family]]
 +
 +==== Hardware Setup ====
 +An ADIS16227/​PCBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N:
 +
 +    ADIS16227/​PCBZ J1 connector Pin 3 (CS)   → YRDKRX62N J8 connector Pin 15
 +    ADIS16227/​PCBZ J1 connector Pin 6 (MOSI) → YRDKRX62N J8 connector Pin 19
 +    ADIS16227/​PCBZ J1 connector Pin 4 (MISO) → YRDKRX62N J8 connector Pin 22
 +    ADIS16227/​PCBZ J1 connector Pin 2 (SCLK) → YRDKRX62N J8 connector Pin 20
 +    ADIS16227/​PCBZ J1 connector Pin 1 (RST)  → YRDKRX62N JN1 connector Pin 16
 +    ADIS16227/​PCBZ J1 connector Pin 7 (GND)  → YRDKRX62N J8 connector Pin 4
 +    ADIS16227/​PCBZ J1 connector Pin 10 (VCC) → YRDKRX62N J8 connector Pin 3
 +
 +{{ :​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rx62n.jpg?​ |}}
 +
 +==== Reference Project Overview ====
 +The reference project runs an offset correction operation, configures the REC_CTRL register and initiates a Manual Time recording. After the process is finished on the LCD are displayed the internal temperature,​ the power supply voltage and the first value of each axis's buffer.
 +
 +{{ :​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rx62n_screen.jpg?​ |}}
 +
 +==== Software Project Setup ====
 +{{page>​rx62n_software_design}}
 +
 +====== More information ======
 +{{page>​more-information}}
resources/tools-software/uc-drivers/renesas/adis16227.1331904188.txt.gz · Last modified: 16 Mar 2012 14:23 by dragosb