Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:tools-software:uc-drivers:renesas:adis16227 [28 Feb 2012 17:08]
dragosb Added the "Downloads" section.
resources:tools-software:uc-drivers:renesas:adis16227 [16 Nov 2012 16:46] (current)
larsc [Evaluation Boards] fixup eval board link
Line 5: Line 5:
  
 ===== Evaluation Boards ===== ===== Evaluation Boards =====
-  * [[adi>​ADIS16227 | ADIS16227/​PCBZ]]+  * [[adi>EVAL-ADIS16227|ADIS16227/​PCBZ]]
  
 ===== Overview ===== ===== Overview =====
Line 16: Line 16:
 **HW Platform(s):​** **HW Platform(s):​**
   * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrl78g13/​index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]]   * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrl78g13/​index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]]
 +  * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrx62n/​index.jsp|Renesas Demo Kit for RX62N (Renesas)]]
 ===== Driver Description ===== ===== Driver Description =====
 The driver contains two parts: The driver contains two parts:
Line 50: Line 50:
   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_generic.zip|ADIS16227 Generic Driver}}   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_generic.zip|ADIS16227 Generic Driver}}
   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rl78g13.zip|ADIS16227 RL78G13 Driver}}   * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rl78g13.zip|ADIS16227 RL78G13 Driver}}
 +  * {{:​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rx62n.zip|ADIS16227 RX62N Driver}}
  
 ====== Renesas RL78G13 Quick Start Guide ====== ====== Renesas RL78G13 Quick Start Guide ======
-This section contains a description of the steps required to run the ADF4118 ​demonstration project on a Renesas RL78G13 platform. ​+This section contains a description of the steps required to run the ADIS16227 ​demonstration project on a Renesas RL78G13 platform. ​
  
 ==== Required Hardware ==== ==== Required Hardware ====
Line 60: Line 61:
 ==== Required Software ==== ==== Required Software ====
   * [[http://​www.iar.com/​en/​Products/​IAR-Embedded-Workbench/​Renesas-RL78/​|IAR Embedded Workbench for Renesas RL78 Kickstart]]   * [[http://​www.iar.com/​en/​Products/​IAR-Embedded-Workbench/​Renesas-RL78/​|IAR Embedded Workbench for Renesas RL78 Kickstart]]
 +  * [[http://​am.renesas.com/​|Applilet3 for RL78G13]]
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
Line 73: Line 75:
  
 {{ :​resources:​tools-software:​uc-drivers:​renesas:​adis16227_pcbz_rl78g13.jpg?​ |}} {{ :​resources:​tools-software:​uc-drivers:​renesas:​adis16227_pcbz_rl78g13.jpg?​ |}}
 +
 +==== Software Setup ====
 +With the //​**Applilet3 for RL78G13**// tool the following peripherals have to be configured:
 +
 +=== CSI10 (Clocked Serial Interface 10) – For the ADIS16227 part and the ST7579 LCD ===
 +Choose to generate the Transmit/​receive function for the CSI10 and configure the interface with the following settings:
 +  * Transfer mode setting: //**Single transfer mode**//
 +  * Data length setting : //**8 bits**//
 +  * Transfer direction setting: //**MSB**//
 +  * Specification of data timing: //**Type 1**//
 +  * Transfer rate setting – Clock mode: //​**Internal clock (master)**//​
 +  * Transfer rate setting – Baudrate: //​**1000000**//​ (bps)
 +  * Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**//
 +  * Uncheck the callback functions.
 +
 +=== TM00 (Timer 00) – For the DelayMs() function === 
 +Configure TM00 as an interval timer:
 +  * Interval timer setting - Interval value(16 bits): //**1**// ms
 +  * Interval timer setting - Uncheck //Generates INTM00 when counting is started//
 +  * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)//
 +
 +=== Watchdog Timer ===
 +Disable the watchdog timer:
 +  * Choose for the Watchdog timer operation setting: //​**Unused**//​ option.
  
 ==== Reference Project Overview ==== ==== Reference Project Overview ====
Line 80: Line 106:
  
 ==== Software Project Setup ==== ==== Software Project Setup ====
-{{page>rl78g13_software_design}}+{{page>rl78g13_software_tutorial}} 
 + 
 +====== Renesas RX62N Quick Start Guide ====== 
 +This section contains a description of the steps required to run the ADIS16227 demonstration project on a Renesas RX62N platform. 
 + 
 +==== Required Hardware ==== 
 +  * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrx62n/​index.jsp|Renesas Demo Kit for RX62N (Renesas)]] 
 +  * [[adi>​ADIS16227 | ADIS16227/​PCBZ (Analog Devices)]] 
 +==== Required Software ==== 
 +  * [[http://​www.renesas.com/​products/​tools/​ide/​ide_hew/​index.jsp|High-performance Embedded Workshop for RX62N family]] 
 +  * [[http://​am.renesas.com/​products/​tools/​middleware_and_drivers/​c_driver_gen/​driver_gen_rpdl/​index.jsp|Renesas Peripheral Driver Library for RX62N family]] 
 + 
 +==== Hardware Setup ==== 
 +An ADIS16227/​PCBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: 
 + 
 +    ADIS16227/​PCBZ J1 connector Pin 3 (CS)   → YRDKRX62N J8 connector Pin 15 
 +    ADIS16227/​PCBZ J1 connector Pin 6 (MOSI) → YRDKRX62N J8 connector Pin 19 
 +    ADIS16227/​PCBZ J1 connector Pin 4 (MISO) → YRDKRX62N J8 connector Pin 22 
 +    ADIS16227/​PCBZ J1 connector Pin 2 (SCLK) → YRDKRX62N J8 connector Pin 20 
 +    ADIS16227/​PCBZ J1 connector Pin 1 (RST)  → YRDKRX62N JN1 connector Pin 16 
 +    ADIS16227/​PCBZ J1 connector Pin 7 (GND)  → YRDKRX62N J8 connector Pin 4 
 +    ADIS16227/​PCBZ J1 connector Pin 10 (VCC) → YRDKRX62N J8 connector Pin 3 
 + 
 +{{ :​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rx62n.jpg?​ |}} 
 + 
 +==== Reference Project Overview ==== 
 +The reference project runs an offset correction operation, configures the REC_CTRL register and initiates a Manual Time recording. After the process is finished on the LCD are displayed the internal temperature,​ the power supply voltage and the first value of each axis's buffer. 
 + 
 +{{ :​resources:​tools-software:​uc-drivers:​renesas:​adis16227_rx62n_screen.jpg?​ |}} 
 + 
 +==== Software Project Setup ==== 
 +{{page>​rx62n_software_design}}
  
 +====== More information ======
 +{{page>​more-information}}
resources/tools-software/uc-drivers/renesas/adis16227.1330445283.txt.gz · Last modified: 28 Feb 2012 17:08 by dragosb