Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:tools-software:uc-drivers:renesas:adf4118_rx62n [02 Feb 2012 16:03] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:adf4118_rx62n [25 Jan 2021 05:24] (current) – update renesas links after their web site update Robin Getz |
---|
The Renesas Demonstration Kit (RDK) for RX62N is an evaluation and demonstration tool for Renesas RX62N microcontrollers. The goal is to provide the user with a powerful debug and demonstration platform targeted at common applications. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using the High-performance Embedded Workshop (HEW) IDE as well as programming the device using the on-board SEGGER J-Link JTAG debugger. | The Renesas Demonstration Kit (RDK) for RX62N is an evaluation and demonstration tool for Renesas RX62N microcontrollers. The goal is to provide the user with a powerful debug and demonstration platform targeted at common applications. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using the High-performance Embedded Workshop (HEW) IDE as well as programming the device using the on-board SEGGER J-Link JTAG debugger. |
| |
{{ :resources:tools-software:renesas:rx62n:yrdkrx62n.jpg? |}} | {{ :resources:tools-software:renesas:rx62n:yrdkrx62n.jpg?400 |}} |
| |
<WRAP centeralign> | |
The Renesas Demonstration Kit (RDK) for RX62N | |
</WRAP> | |
| |
The [[adi>ADF4118]] is frequency synthesizer which can be used to implement local oscillators in the up-conversion and down-conversion sections of wireless receivers and transmitters. It consists of a low-noise digital PFD (Phase Frequency Detector), a precision charge pump, a programmable reference divider, programmable A and B counters and a dual-modulus prescaler (P/P+1). The A (5-bit) and B (13-bit) counters, in conjunction with the dual modulus prescaler (P/P+1), implement an N divider (N= BP+A). In addition, the 14-bit reference counter (R Counter), allows selectable REFIN frequencies at the PFD input. A complete PLL (Phase-Locked Loop) can be implemented if the synthesizer is used with an external loop filter and VCO (Voltage Controlled Oscillator). | The [[adi>ADF4118]] is frequency synthesizer which can be used to implement local oscillators in the up-conversion and down-conversion sections of wireless receivers and transmitters. It consists of a low-noise digital PFD (Phase Frequency Detector), a precision charge pump, a programmable reference divider, programmable A and B counters and a dual-modulus prescaler (P/P+1). The A (5-bit) and B (13-bit) counters, in conjunction with the dual modulus prescaler (P/P+1), implement an N divider (N= BP+A). In addition, the 14-bit reference counter (R Counter), allows selectable REFIN frequencies at the PFD input. A complete PLL (Phase-Locked Loop) can be implemented if the synthesizer is used with an external loop filter and VCO (Voltage Controlled Oscillator). |
| |
* [[adi>ADF4118|ADF4118 Product Info]] - pricing, samples, datasheet | * [[adi>ADF4118|ADF4118 Product Info]] - pricing, samples, datasheet |
* [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/yrdkrx62n.jsp | Renesas Demo Kit for RX62N]] - pricing, documentation | * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n | Renesas Demo Kit for RX62N]] - pricing, documentation |
| |
====== Project Description ====== | ====== Project Description ====== |