This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7980 [27 May 2013 16:03] – added RENESAS RL78G14 QUICK START GUIDE and RL78G14 source code downloads Lucian Sin | resources:tools-software:uc-drivers:renesas:ad7980 [28 May 2013 09:00] – [Reference Project Overview] Lucian Sin | ||
---|---|---|---|
Line 46: | Line 46: | ||
<WRAP round important 80%> | <WRAP round important 80%> | ||
* The reference voltage for the AD7980 is 2.5V. | * The reference voltage for the AD7980 is 2.5V. | ||
- | * If you want to use another reference voltage, you will need to modify the vRef parameter in ‘AD7980_ConvertToVolts()’ function from ‘main.c’. The range for VREF is 2.4V ≤ VREF ≤ 5.1V. | + | * If you want to use another reference voltage, you will need to modify the vRef parameter in ‘AD7980_ConvertToVolts()’ function from ‘PmodAD4.c’. The range for VREF is 2.4V ≤ VREF ≤ 5.1V. |
</ | </ | ||