This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:uc-drivers:renesas:ad7980 [24 Jan 2021 17:18] – Fix bad links Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7980 [27 Jan 2021 23:00] (current) – use interwiki links Robin Getz | ||
---|---|---|---|
Line 22: | Line 22: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[https:// | * [[https:// | ||
- | * [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] | + | * [[adi> |
==== Required Software ==== | ==== Required Software ==== | ||
Line 28: | Line 28: | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | A [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] has to be connected to the PMOD1 connector, pins 1 to 6 (see image below). | + | A [[adi> |
{{ : | {{ : | ||
Line 55: | Line 55: | ||
====== Renesas RL78G14 Quick Start Guide ====== | ====== Renesas RL78G14 Quick Start Guide ====== | ||
- | This section contains a description of the steps required to run the AD7980 demonstration project on a Renesas RL78G14 platform using the [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]]. | + | This section contains a description of the steps required to run the AD7980 demonstration project on a Renesas RL78G14 platform using the [[adi> |
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[https:// | * [[https:// | ||
- | * [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] | + | * [[adi> |
==== Required Software ==== | ==== Required Software ==== | ||
Line 66: | Line 66: | ||
<WRAP round info 80%> | <WRAP round info 80%> | ||
- | The AD7980 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD7980 Driver**, | + | The AD7980 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD7980 Driver**, |
All three parts have to be downloaded. | All three parts have to be downloaded. | ||
</ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | A [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] has to be connected to the PMOD1 connector, pins 1 to 6 (see image below). | + | A [[adi> |
{{ : | {{ : | ||
Line 103: | Line 103: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[https:// | * [[https:// | ||
- | * [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] | + | * [[adi> |
==== Required Software ==== | ==== Required Software ==== | ||
Line 110: | Line 110: | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | A [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: | + | A [[adi> |
PmodAD4 Pin 1 (CS) → YRDKRX62N J8 connector Pin 15 | PmodAD4 Pin 1 (CS) → YRDKRX62N J8 connector Pin 15 |