This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad5629r [09 May 2012 15:12] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad5629r [01 Jun 2012 12:45] – Added the "More Information" section Dragos Bogdan | ||
---|---|---|---|
Line 46: | Line 46: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{: | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 99: | Line 100: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RX62N Quick Start Guide ====== | ||
+ | |||
+ | This section contains a description of the steps required to run the AD5629R demonstration project on a Renesas RX62N platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[adi> | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | An EVAL-AD5629REBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: | ||
+ | |||
+ | EVAL-AD5629RSDZ J6 connector Pin SCL | ||
+ | EVAL-AD5629RSDZ J7 connector Pin SDA | ||
+ | EVAL-AD5629RSDZ J8 connector Pin \LDAC (LDAC) | ||
+ | EVAL-AD5629RSDZ J9 connector Pin \CLR (CLR) → YRDKRX62N J8 connector Pin 25 | ||
+ | | ||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project: | ||
+ | The reference project powers-up all DAC channels, displays the content of the power register and starts to generate a saw-tooth wave. | ||
+ | |||
+ | {{ : | ||
+ | | ||
+ | ==== Software Project Setup ==== | ||
+ | {{page> | ||
+ | |||
+ | ====== More information ====== | ||
+ | {{page> |