Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Last revision Both sides next revision
resources:tools-software:uc-drivers:renesas:ad5628 [06 Nov 2012 17:07]
DragosB Removed applilet3 content / updated drivers.
resources:tools-software:uc-drivers:renesas:ad5628 [28 May 2013 15:11]
LucianS added RENESAS RL78G14 QUICK START GUIDE and RL78G14 source code downloads
Line 8: Line 8:
 ===== Downloads ===== ===== Downloads =====
  
-<WRAP round download ​30%>+<WRAP round download ​80%>
   * {{:​resources:​tools-software:​uc-drivers:​ad5628_generic.zip|AD5628 Generic Driver}}   * {{:​resources:​tools-software:​uc-drivers:​ad5628_generic.zip|AD5628 Generic Driver}}
   * {{:​resources:​tools-software:​uc-drivers:​renesas:​ad5628_rl78g13.zip|AD5628 RL78G13 Driver}}   * {{:​resources:​tools-software:​uc-drivers:​renesas:​ad5628_rl78g13.zip|AD5628 RL78G13 Driver}}
   * {{:​resources:​tools-software:​uc-drivers:​renesas:​ad5628_rx62n.zip|AD5628 RX62N Driver}}   * {{:​resources:​tools-software:​uc-drivers:​renesas:​ad5628_rx62n.zip|AD5628 RX62N Driver}}
 +  * **AD5628 Driver: ​           ** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​drivers/​AD5628
 +  * **PmodDA4 Demo for RL78G14: ** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​Renesas/​RL78G14/​PmodDA4
 +  * **RL78G14 Common Drivers: ​  ** https://​github.com/​analogdevicesinc/​no-OS/​tree/​master/​Renesas/​RL78G14/​Common
 </​WRAP>​ </​WRAP>​
  
Line 26: Line 29:
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
-A PmodDA4 has to be connected to the PMOD1 connector.+A PmodDA4 has to be connected to the PMOD1 connector, pins 1 to 6 (see image below).
  
 {{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_da4_rl78g13.jpg?​ |}} {{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_da4_rl78g13.jpg?​ |}}
Line 35: Line 38:
   * to channel B, a value corresponding to 1/4 of Full Scale;   * to channel B, a value corresponding to 1/4 of Full Scale;
   * to channel C, a value corresponding to 1/8 of Full Scale.   * to channel C, a value corresponding to 1/8 of Full Scale.
 +
 +<WRAP round important 80%>
 +\\
 +The voltage reference is 2.5V.
 +\\
 +</​WRAP>​
  
 {{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_da4_rl78g13_screen.jpg?​ |}} {{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_da4_rl78g13_screen.jpg?​ |}}
Line 40: Line 49:
 ==== Software Project Tutorial ==== ==== Software Project Tutorial ====
 {{page>​rl78g13_software_tutorial_without_applilet3}} {{page>​rl78g13_software_tutorial_without_applilet3}}
 +
 +====== Renesas RL78G14 Quick Start Guide ======
 +This section contains a description of the steps required to run the AD5628 demonstration project on a Renesas RL78G14 platform using the PmodDA4.
 +
 +==== Required Hardware ====
 +  * [[http://​am.renesas.com/​products/​tools/​introductory_evaluation_tools/​renesas_demo_kits/​yrdkrl78g14/​index.jsp|Renesas Demo Kit for RL78G14 (Renesas)]]
 +  * [[http://​www.digilentinc.com/​Products/​Detail.cfm?​Prod=PMOD-DA4|PmodDA4]]
 +
 +==== Required Software ====
 +  * [[http://​www.iar.com/​en/​Products/​IAR-Embedded-Workbench/​Renesas-RL78/​|IAR Embedded Workbench for Renesas RL78 Kickstart]]
 +  * The AD5628 demonstration project for the Renesas RL78G14 platform.
 +
 +<WRAP round info 80%>
 +The AD5628 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD5628 Driver**, ​ the **PmodDA4 Demo for RL78G14** and the **RL78G14 Common Drivers**.
 +
 +All three parts have to be downloaded.
 +</​WRAP>​
 +==== Hardware Setup ====
 +A PmodDA4 has to be connected to the PMOD1 connector, pins 1 to 6 (see image below).
 +
 +{{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_da4_rl78g14.jpg?​ |}}
 +
 +
 +==== Reference Project Overview ====
 +The reference project initializes the AD5628 part and writes:
 +  * to channel A, a value corresponding to 1/2 of Full Scale;
 +  * to channel B, a value corresponding to 1/4 of Full Scale;
 +  * to channel C, a value corresponding to 1/8 of Full Scale.
 +
 +<WRAP round important 80%>
 +\\
 +The voltage reference is 2.5V.
 +\\
 +</​WRAP>​
 +
 +{{ :​resources:​tools-software:​uc-drivers:​renesas:​pmod_da4_rl78g14_screen.jpg?​ |}}
 +
 +
 +==== Software Project Tutorial ====
 +{{page>​rl78g14_software_tutorial}}
 +
  
 ====== Renesas RX62N Quick Start Guide ====== ====== Renesas RX62N Quick Start Guide ======
resources/tools-software/uc-drivers/renesas/ad5628.txt · Last modified: 22 Jul 2019 13:38 by AndreiD1994