Wiki

This version (09 Oct 2012 09:21) was approved by Dragos Bogdan.The Previously approved version (23 Jul 2012 16:51) is available.Diff

This section presents the steps for developing a chipKIT application that will run on the Digilent Cerebot MX3cK development board for controlling and monitoring the operation of the ADI part.

  • Under your Sketchbook directory create a folder called “Libraries”; this folder may already exist.
  • Unzip the downloaded file in the libraries folder.
  • Run the MPIDE environment.
  • You should see the new library under Sketch→Import Library, under Contributed.

  • Also you should see under File→Examples the demo project for the ADI library.
  • Select the ADIDriver example.

  • Select the Cerebot MX3cK board from Tools→Board.
  • Select the corresponding Serial Communication Port from Tools→Serial Port
  • The project is ready to be uploaded on the development board.

resources/tools-software/uc-drivers/microchip/arduino_software_design.txt · Last modified: 09 Oct 2012 09:21 by Dragos Bogdan