This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:uc-drivers:microchip:adxrs453 [01 Oct 2012 16:30] – created Dragos Bogdan | resources:tools-software:uc-drivers:microchip:adxrs453 [22 Jul 2019 14:15] (current) – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{: | + | <WRAP round download 80%> |
- | * {{: | + | |
* {{: | * {{: | ||
- | * {{: | + | * {{: |
+ | * **ADXRS453 Driver:** https:// | ||
+ | * **PmodGYRO2 Demo for PIC32MX320F128H: | ||
+ | * **PIC32MX320F128H Common Drivers:** https:// | ||
+ | </ | ||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
Line 17: | Line 20: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[http:// | * [[http:// | ||
- | * PmodGYRO2 | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * The ADXRS453 demonstration project for PIC32MX320F128H. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The ADXRS453 demonstration project for PIC32MX320F128H consists of three parts: the **ADXRS453 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 29: | Line 39: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following | + | The following |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | temperature? | + | | temperature? |
- | | start= | + | | measure! |
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | + | The following image shows a generic |
{{ : | {{ : | ||
Line 63: | Line 73: | ||
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | temperature? | + | | temperature? |
| start= | Starts measurement. Accepted value: 1. | | | start= | Starts measurement. Accepted value: 1. | | ||
Line 74: | Line 84: | ||
{{page>: | {{page>: | ||
- | ====== Digilent Cerebot MX3cK Quick Start Guide - Arduino | + | ====== Digilent Cerebot MX3cK Quick Start Guide - chipKIT Project |
- | This section contains a description of the steps required to run the ADXRS453 | + | This section contains a description of the steps required to run the ADXRS453 |
==== Required Hardware ==== | ==== Required Hardware ==== | ||
Line 90: | Line 100: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following commands were implemented in this version of ADXRS453 | + | Following commands were implemented in this version of ADXRS453 |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | |