This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:uc-drivers:microchip:adxl345 [28 Sep 2012 13:56] – Added the generic driver. Dragos Bogdan | resources:tools-software:uc-drivers:microchip:adxl345 [22 Jul 2019 09:41] (current) – Update driver link Andrei Drimbarean | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== ADXL345 - No-OS Driver for Microchip Microcontroller Platforms ====== | ||
{{page>: | {{page>: | ||
Line 6: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{: | + | <WRAP round download 80%> |
- | * {{: | + | |
* {{: | * {{: | ||
- | * {{: | + | * {{: |
+ | * **ADXL345 Driver: | ||
+ | * **PmodACL Demo for PIC32MX320F128H: | ||
+ | * **PIC32MX320F128H Common Drivers: | ||
+ | </ | ||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
Line 21: | Line 26: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * The ADXL345 demonstration project for PIC32MX320F128H. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The ADXL345 demonstration project for PIC32MX320F128H consists of three parts: the **ADXL345 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
+ | |||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 32: | Line 45: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following | + | The following |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | communication= | Selects the communication interface. Accepted values: 0(I2C),1(SPI). | | + | | communication= | Selects the communication interface. Accepted values:\\ 0 - SPI.\\ 1 - I2C. | |
| communication? | | communication? | ||
- | | acceleration? | + | | acceleration? |
+ | | accelerationX? | ||
+ | | accelerationY? | ||
+ | | accelerationZ? | ||
| interrupts? | Displays the state of the interrupts. | | | interrupts? | Displays the state of the interrupts. | | ||
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | + | The following image shows a generic |
{{ : | {{ : | ||
Line 85: | Line 101: | ||
{{page>: | {{page>: | ||
- | ====== Digilent Cerebot MX3cK Quick Start Guide - Arduino | + | ====== Digilent Cerebot MX3cK Quick Start Guide - chipKIT Project |
- | This section contains a description of the steps required to run the ADXL345 | + | This section contains a description of the steps required to run the ADXL345 |
==== Required Hardware ==== | ==== Required Hardware ==== |