This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:uc-drivers:microchip:adt7420 [27 Jun 2013 09:26] – [Required Software] Lucian Sin | resources:tools-software:uc-drivers:microchip:adt7420 [22 Jul 2019 14:32] (current) – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 10: | Line 10: | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
* {{: | * {{: | ||
- | * **ADT7420 Driver: | + | * **ADT7420 Driver: |
* **PmodTMP2 Demo for PIC32MX320F128H: | * **PmodTMP2 Demo for PIC32MX320F128H: | ||
* **PIC32MX320F128H Common Drivers: | * **PIC32MX320F128H Common Drivers: | ||
Line 27: | Line 27: | ||
<WRAP round info 80%> | <WRAP round info 80%> | ||
- | The ADT7420 demonstration project for the Digilent Cerebot MX3cK platform | + | The ADT7420 demonstration project for PIC32MX320F128H |
All three parts have to be downloaded. | All three parts have to be downloaded. | ||
Line 41: | Line 41: | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
| reset! | Resets the ADT7420. | | | reset! | Resets the ADT7420. | | ||
- | | mode= | Sets the operational mode for ADT7420. Accepted values: 0 - 3 | | + | | mode= | Sets the operational mode for ADT7420. Accepted values:\\ 0 - Continuos conversions.\\ 1 - One shot.\\ 2 - 1 SPS mode.\\ |
| mode? | Displays the selected operational mode. | | | mode? | Displays the selected operational mode. | | ||
- | | resolution= | Sets the resolution for ADT7420. Accepted values: 0 - 1 | | + | | resolution= | Sets the resolution for ADT7420. Accepted values:\\ 0 - 13 bits resolution.\\ |
| resolution? | Displays the selected resolution. | | | resolution? | Displays the selected resolution. | | ||
| temperature? | | temperature? | ||
Line 51: | Line 51: | ||
The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral. | The following image shows a generic list of commands in a serial terminal connected to processor’s UART peripheral. | ||
{{ : | {{ : | ||
- | |||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page>: | {{page>: |