This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:microchip:adp5589 [01 Oct 2012 16:11] – created Dragos Bogdan | resources:tools-software:uc-drivers:microchip:adp5589 [28 Jun 2013 15:03] – [Reference Project Overview] Lucian Sin | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{: | + | <WRAP round download 80%> |
- | * {{: | + | |
* {{: | * {{: | ||
+ | * **ADP5589 Driver: | ||
+ | * **PmodIOXP Demo for PIC32MX320F128H: | ||
+ | * **PIC32MX320F128H Common Drivers: | ||
+ | </ | ||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
Line 21: | Line 24: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * The ADP5589 demonstration project for PIC32MX320F128H. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The ADP5589 demonstration project for PIC32MX320F128H consists of three parts: the **ADP5589 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | A PmodIOXP has to be connected to the J2 connector of Cerebot MX3cK development board. | + | A PmodIOXP has to be connected to the J2 connector of Cerebot MX3cK development board. For this demonstration project, PmodKYPD must be connected to J2 connector of PmodIOXP, because the PWM signal is mapped on J1 connector, pin 4. |
{{ : | {{ : | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following | + | The following |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
- | | pwmOnTime= | On time of the PWM pulse. Accepted values: | + | | pwmOnTime= | On time of the PWM pulse. Accepted values:\\ 1 .. 65535[us] - time when the signal is high. | |
- | | pwmOffTime= | Off time of the PWM pulse. Accepted values: | + | | pwmOffTime= | Off time of the PWM pulse. Accepted values:\\ 1 .. 65535[us] - time when the signal is low. | |
- | | lastKey? | Displays the last key which was pressed | | + | | keyPressed? | Displays the last key which was pressed. | |
+ | | keyReleased? | ||
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | + | The following image shows a generic |
{{ : | {{ : | ||
- | |||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page>: | {{page>: |