This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:microchip:ad5933 [09 Oct 2012 09:18] – Replaced Arduino with chipKIT. Dragos Bogdan | resources:tools-software:uc-drivers:microchip:ad5933 [04 Jul 2013 14:42] – [Reference Project Overview] Lucian Sin | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | * {{: | + | <WRAP round download 80%> |
- | * {{: | + | |
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **AD5933 Driver:** https:// | ||
+ | * **PmodIA Demo for PIC32MX320F128H: | ||
+ | * **PIC32MX320F128H Common Drivers:** https:// | ||
+ | </ | ||
====== Digilent Cerebot MX3cK Quick Start Guide ====== | ====== Digilent Cerebot MX3cK Quick Start Guide ====== | ||
Line 17: | Line 20: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[http:// | * [[http:// | ||
- | * PmodIA | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * The AD5933 demonstration project for PIC32MX320F128H. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The AD5933 demonstration project for PIC32MX320F128H consists of three parts: the **AD5933 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
+ | |||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 29: | Line 40: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | Following | + | The following |
^ Command ^ Description ^ | ^ Command ^ Description ^ | ||
| help? | Displays all available commands. | | | help? | Displays all available commands. | | ||
| temperature? | | temperature? | ||
- | | startFreq= | Start frequency parameter. Accepted values: | + | | startFreq= | Sets the start frequency parameter. Accepted values:\\ 1 000 .. 100 000 [Hz] - set parameter. | |
- | | incFreq= | Frequency | + | | incFreq= | Sets the frequency |
- | | incNum= | Number | + | | incNum= | Sets the number |
| sweepParam? | Displays all three sweep parameters. | | | sweepParam? | Displays all three sweep parameters. | | ||
- | | calibImpedance= | Calibration | + | | calibImpedance= | Sets the calibration |
| impedance? | Displays the measured impedance. | | | impedance? | Displays the measured impedance. | | ||
| currentFreq? | | currentFreq? | ||
Line 43: | Line 54: | ||
Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. | ||
- | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | + | The following image shows a generic |
{{ : | {{ : | ||
- | |||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page>: | {{page>: |