Wiki

This version is outdated by a newer approved version.DiffThis version (13 Apr 2023 09:48) was approved by Jose Ramon San Buenaventura.

This is an old revision of the document!


MAX9611 - No-OS Driver

Supported Devices

Evaluation Boards

Overview

The MAX9611 / MAX9612 are high-side current-sense amplifiers with an integrated 12-bit ADC and a gain block that can be configured either as an op amp or comparator, making these devices ideal for a number of industrial and automotive applications.

The high-side, current-sense amplifiers operate over a wide 0 V to 60 V input common-mode voltage range. The programmable full-scale voltage (440 mV, 110 mV, and 55 mV) of these amplifiers offers wide dynamic range, accurate current measurement, and application flexibility in choosing sense resistor values. A choice of either an internal op amp or a comparator is provided to the user.

The internal amplifier can be used to limit the inrush current or to create a current source in a closed-loop system. The comparator can be used to monitor fault events for fast response.

An I2C-controlled 12-bit, 500 sps analog-to-digital converter (ADC) can be used to read the voltage across the sense resistor (VSENSE), the input common-mode voltage (VRSCM), op amp/comparator output (VOUT), op amp/ comparator reference voltage (VSET), and internal die temperature.

The I2C bus is compatible with 1.8 V and 3.3 V logic, allowing modern microcontrollers to interface to it. The MAX9611 features a noninverting input-to-output configuration, while the MAX9612 features an inverting input-to-output configuration.

Applications

  • Hybrid automotive power supplies
  • Server backplanes
  • Base station PA control
  • Base station feeder cable bias tee
  • Telecom cards
  • Battery-operated equipment

ADI No-OS

The goal of the ADI Microcontroller No-OS is to provide reference projects for lower end processors, which can't run Linux or aren't running a specific operating system, and to help those customers using microcontrollers with ADI parts. ADI No-OS offers generic drivers, which can be used as a base for any microcontroller platform and also example projects, which are using these drivers on various microcontroller platforms.

For more information about ADI No-OS and supported microcontroller platforms, visit the No-OS User Guide.

MAX9611 ADI No-OS driver

Driver Source Code

The source code for MAX9611 driver can be found here:

This driver also uses the ADI utility library, so make sure you also add the necessary files to your project. The source code for the utility library can be found here:

To use the MAX9611 No-OS driver, you need to provide the specific implementation for the communication APIs and the specific types they use.
If the SPI communication is chosen, there are three functions which are called by the MAX9611 driver and have to be implemented:

no_os_i2c_init() initializes the communication peripheral.
no_os_i2c_write() writes data to the device.
no_os_i2c_read() reads data from the device.
no_os_i2c_remove() deinitializes the communication peripheral.

And there are two data types that have to be defined:

no_os_i2c_desc structure holding the I2C descriptor
no_os_i2c_init_param structure holding the parameters for I2C initialization

An example of a header file containing the prototypes of the functions which have to be implemented, along with some generic data types they are using, can be found below:

Code Documentation

Source code documentation for the driver is automatically generated using the Doxygen tool and can be accessed in these links:

Device Configuration

Driver Initialization

To use the device, you need to provide the support for the communication protocol (I2C) as mentioned above.

The first API function to be called is max9611_addr_gen to generate the corresponding device's slave address. Once a proper address is generated, use the function max9611_init to initialize the device and make sure that it returns 0. This indicates a successful driver initialization.

Device Address Generation

The MAX9611 / MAX9612 have the provision for multiple I2C slave addresses via the A0 and A1 pins. To generate the proper address, supply the voltage level going into pins A0 and A1 to the max9611_addr_gen function.

The header file of the MAX9611 driver provides an enumeration for the valid A0 and A1 input voltage level values. There are a total of 16 valid slave address combinations that can be generated depending on the voltage level supplied to the address pin. For reference, refer to Table 2 of the MAX9611 data sheet.

Output Amplifier / Comparator Configuration

The MAX9611 contains an internally selectable op amp and comparator whose inputs are the current sense amplifier with a 2.5 gain and the SET pin. By using the max9611_set_mode and max9611_get_mode functions, the user would be able to set and obtain the configuration of the OUT pin, respectively. The header file contains the enumerations pertaining to the valid operating modes.

Configurable Analog-to-Digital Converter (ADC)

The MAX9611 contains an internal dual-slope integrating 12-bit ADC with a 2 mS conversion time. This ADC is also compatible with 1.8 V or 3.3 V I2C logic level buses. This ADC contains an internal MUX to allow selection between the following measurements: input sense voltage, input common-mode voltage, SET pin voltage, OUT pin voltage, and die temperature.

Similarly, the mux configuration can be set or read through the max9611_set_mux and max9611_get_mux driver functions. The max9611_set_mux function also allows a burst read of all viable channels, which might be useful for certain applications. The valid enumerations corresponding to each usable mode can be seen below:

MAX9611_CONF_SENSE_1X measure Current Sense Amplifier Output with gain = 1
MAX9611_CONF_SENSE_4X measure Current Sense Amplifier Output with gain = 4
MAX9611_CONF_SENSE_8X measure Current Sense Amplifier Output with gain = 8
MAX9611_CONF_IN_COM_MODE measure input common mode voltage
MAX9611_CONF_OUT_ADC measure OUT pin voltage
MAX9611_CONF_SET_ADC measure SET pin voltage
MAX9611_CONF_TEMP measure internal die temperature
MAX9611_FAST_MODE measure all channels in fast mode (uses last gain setting)

Once the mux configuration has been set, the selected channel measurement can be read using the max9611_get_raw function.

The max9611_get_raw function only allows reading of single channel measurements i.e., Current Sense Amplifier (CSA) input only. Setting the device to fast mode via max9611_set_mux for a burst read of multiple channels will require a multi-byte register read starting from the CSA MSB register (0x00) up to the Temp LSB register (0x09) using the max9611_read function.


Die Temperature Measurement
By configuring the internal mux using max9611_set_mux function, the die temperature of the MAX9611 can also be measured. The temperature measurement ranges from -40°C to +125°C with a 0.48°C step size. The temperature measurement is encoded using 9 bits in two's complement format.

Refer to Table 1 of MAX9611 data sheet for the converting the LSB read into its corresponding temperature measurement.


Watchdog/Retry/Latch Functionality

The MAX9611's internal digital block sports a watchdog function for handling false fault transients, applicable for both op amp and comparator operating modes. Different time delay options for the comparator are configured in CONTROL REGISTER 2 through the corresponding driver functions:

max9611_set_delay configures the watchdog delay time
max9611_get_delay acquires the configured watchdog delay time
max9611_set_retry configure the watchdog retry delay time
max9611_get_retry acquires the configured watchdog retry delay time


The valid delay times for the watchdog delay and retry delay times are as follows:

Watchdog Delay Times

MAX9611_1MS 1 mS watchdog delay time (default)
MAX9611_100US 100 µS watchdog delay time

Watchdog Retry Delay Times

MAX9611_50MS 50 mS watchdog retry delay time (default)
MAX9611_10MS 10 mS watchdog retry delay time

During Normal Operation (MAX9611_NORMAL_MODE), the internal amplifier output depends on its inputs: the CSA output and the SET pin voltage level. This internal amplifier can act as a comparator for open-loop configurations.

For op amp (MAX9611_OPAMP_MODE) or comparator (MAX9611_COMPARATOR_MODE), the comparator output ensures the CSA output stays above the SET voltage level for a watchdog delay time, and then latches on to this state. The retry delay time dictates the time taken before the comparator state is reset and the cycle repeats.

For more information on this, refer to the MAX9611 data sheet under the Watchdog/Latch/Retry Functionality section and other related sections.

Power Down Options

To save power, one may use the max9611_shutdown function resulting in a 5 µA supply current drawn. Alternatively, this function can also be used to bring the component back to its 'power on' state.

Driver Initialization Example

Example Initialization Using Maxim SDK as Platform

	int ret;

	uint8_t mux_conf[] = {
		MAX9611_CONF_SENSE_1X,
		MAX9611_CONF_SENSE_4X,
		MAX9611_CONF_SENSE_8X,
		MAX9611_CONF_IN_COM_MODE,
		MAX9611_CONF_OUT_ADC,
		MAX9611_CONF_SET_ADC,
		MAX9611_CONF_TEMP,
		MAX9611_FAST_MODE,
	};

	uint8_t mode_conf[] = {
		MAX9611_NORMAL_MODE,
		MAX9611_OPAMP_MODE,
		MAX9611_COMPARATOR_MODE,
	};

	uint8_t delays[] = {
		MAX9611_1MS,
		MAX9611_100US,
	};

	uint8_t retries[] = {
		MAX9611_50MS,
		MAX9611_10MS,
	};

	struct max_i2c_init_param max9611_extra = {
		.vssel = MXC_GPIO_VSSEL_VDDIOH,
	};

	struct max9611_init_param max9611_ip = {
		.i2c_init.device_id = 0,
		.i2c_init.max_speed_hz = MAX_I2C_STD_MODE,
		.i2c_init.extra = &max9611_extra,
		.i2c_init.platform_ops = &max_i2c_ops,
	};

	ret = max9611_addr_gen(&max9611_ip, MAX9611_ZERO_VCC, MAX9611_ZERO_VCC);
	if (ret)
		return ret;

	struct max9611_dev *max9611_device;

	ret = max9611_init(&max9611_device, max9611_ip);
	if (ret)
		return ret;

	while (1){
		uint16_t raw_val;
		int mux_cnt = 0, mode_cnt = 0, dcnt = 0, rcnt = 0;

		for (int i = 0; i < NO_OS_ARRAY_SIZE(mux_conf); i++) {
			enum max9611_mux_conf mux, mux_new;
			ret = max9611_get_mux(max9611_device, &mux);
			if (ret)
				return ret;

			ret = max9611_set_mux(max9611_device, mux_conf[i]);
			if (ret)
				return ret;

			ret = max9611_get_mux(max9611_device, &mux_new);
			if (ret)
				return ret;

			ret = max9611_get_raw(max9611_device, &raw_val);
			if (ret)
				return ret;

			if (mux_conf[i] != mux_new)
				mux_cnt++;
		}

		for (int i = 0; i < NO_OS_ARRAY_SIZE(mode_conf); i++) {
			enum max9611_mode_conf mode, mode_new;
			ret = max9611_get_mode(max9611_device, &mode);
			if (ret)
				return ret;

			ret = max9611_set_mode(max9611_device, mode_conf[i]);
			if (ret)
				return ret;

			ret = max9611_get_mode(max9611_device, &mode_new);
			if (ret)
				return ret;

			if (mode_conf[i] != mode_new)
				mode_cnt++;
		}

		for (int i = 0; i < NO_OS_ARRAY_SIZE(delays); i++) {
			enum max9611_delay_time dtime, dtime_new;
			ret = max9611_get_delay(max9611_device, &dtime);
			if (ret)
				return ret;

			ret = max9611_set_delay(max9611_device, delays[i]);
			if (ret)
				return ret;

			ret = max9611_get_delay(max9611_device, &dtime_new);
			if (ret)
				return ret;

			if (delays[i] != dtime_new)
				dcnt++;
		}

		for (int i = 0; i < NO_OS_ARRAY_SIZE(retries); i++) {
			enum max9611_retry_time rtime, rtime_new;
			ret = max9611_get_retry(max9611_device, &rtime);
			if (ret)
				return ret;

			ret = max9611_set_retry(max9611_device, retries[i]);
			if (ret)
				return ret;

			ret = max9611_get_retry(max9611_device, &rtime_new);
			if (ret)
				return ret;

			if (retries[i] != rtime_new)
				rcnt++;
		}


		ret = max9611_shutdown(max9611_device, true);
		if (ret)
			return ret;

		ret = max9611_shutdown(max9611_device, false);
		if (ret)
			return ret;
	}	



resources/tools-software/uc-drivers/max9611.1681372078.txt.gz · Last modified: 13 Apr 2023 09:47 by Jose Ramon San Buenaventura