This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:tools-software:uc-drivers:max31865 [18 Apr 2023 11:22] Jose Ramon San Buenaventura |
resources:tools-software:uc-drivers:max31865 [19 Apr 2023 02:45] Marc Sosa |
||
---|---|---|---|
Line 93: | Line 93: | ||
</WRAP> | </WRAP> | ||
\\ | \\ | ||
- | === Conversion Mode Configuration === | + | === Fault Threshold Configuration === |
The High Fault Threshold and Low Fault Threshold registers select the trip thresholds for RTD fault detection. The results of RTD conversions are compared with the values in these registers to generate the “Fault” bits in the Fault Status register. The RTD Data Registers, High Fault Threshold Registers, and Low Fault Threshold Registers all have the same format. | The High Fault Threshold and Low Fault Threshold registers select the trip thresholds for RTD fault detection. The results of RTD conversions are compared with the values in these registers to generate the “Fault” bits in the Fault Status register. The RTD Data Registers, High Fault Threshold Registers, and Low Fault Threshold Registers all have the same format. | ||