Wiki

This version is outdated by a newer approved version.DiffThis version (27 Sep 2022 17:22) was approved by Darius B.The Previously approved version (25 May 2022 10:31) is available.Diff

This is an old revision of the document!


MAX31855 Driver

Supported devices

Overview

The MAX31855 performs cold-junction compensation and digitizes the signal from a K-, J-, N-, T-, S-, R-, or E-type thermocouple. The data is output in a signed 14-bit, SPI-compatible, read-only format. This converter resolves temperatures to 0.25°C, allows readings as high as +1800°C and as low as -270°C, and exhibits thermocouple accuracy of ±2°C for temperatures ranging from -200°C to +700°C for K-type thermocouples.

The MAX31855 interfaces to most microcontrollers, by using a SPI interface.

Applications

  • Industrial
  • Appliances
  • HVAC

ADI No-OS

The goal of ADI Microcontroller No-OS is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. ADI No-OS offers generic drivers which can be used as a base for any microcontroller platform and also example projects which are using these drivers on various microcontroller platforms.

For more information about ADI No-OS and supported microcontroller platforms see: no-OS

MAX31855 ADI No-OS Driver

The source code for ADXL355 driver can be found here:

The driver also uses the ADI util library, so make sure you also add the necessary files in your project. The source code for the util library can be found here:

In order to be able to use this driver you will have to provide the specific implementation for the communication APIs and the specific types they use. If the SPI communication is chosen, there are three functions which are called by the MAX31855 driver and have to be implemented:

  • no_os_spi_init() – initializes the communication peripheral.
  • no_os_spi_write_and_read() – writes and reads data to/from the device.
  • no_os_spi_remove() – free the communication peripheral descriptor.

And there are two data types that have to be defined:

  • no_os_spi_desc - structure holding the SPI descriptor
  • no_os_spi_init_param - structure holding the parameters for SPI initialization

An example of a header file containing the prototypes of the functions which have to be implemented, along with some generic data types they are using can be found below:

MAX31855 Code Driver Documentation

Source code documentation for the driver is automatically generated using the Doxygen tool and it is available below:

MAX31855 Device Configuration

Driver initialization

The first step before using the driver is to call the max31855_init function, which, in this case, will only initialize the SPI interface. After that (if the init function returns 0), the driver is fully configured, and you will be able to read samples from the device.

The MAX31855 doesn't support any additional configuration. The device only has 1 read-only register.

MAX31855 Device Measurements

Temperature reading

The MAX31855 continuously performs temperature readings as long as it's powered on. To read a temperature sample, the CS pin must be pulled low, which will result in a register update and read.

The API function used for reading a temperature sample is max31855_read_temp, which will provide a value for both cold (the chip's temperature) and hot (the probe's temperature) junctions. These are represented in a integer/decimal form. The unit for the integer part is degrees Celsius. The decimal part will have to be divided by either MAX31855_THERMOCOUPLE_TEMP_DEC_DIV or MAX31855_INTERNAL_TEMP_DEC_DIV to obtain the value in degrees Celsius. The cold junction compensation is already applied.

The raw values can be obtained by using the max31855_read_raw function, and then applying the MAX31855_GET_INTERNAL_TEMP or MAX31855_GET_THERMOCOUPLE_TEMP macros on the val parameter (the register's raw value).

These functions will return an error if any fault bit is set.

MAX31855 Driver Usage Example

int ret;
struct max31855_decimal internal;
struct max31855_decimal thermocouple;

struct max31855_dev *dev;
struct max31855_init_param max31855_param = {
	.spi_init = spi_param
};

ret = max31855_init(&dev, &max31855_param);
if (ret)
        return ret;
ret = max31855_read_temp(dev, &thermocouple, &internal);
if (ret)
        return ret;

ADI IIO No-OS

MAX31855 IIO No-OS driver

The MAX31855 IIO driver comes on top of MAX31855 driver and offers support for interfacing IIO clients through IIO lib.

ADXL355 IIO Driver Source Code

The source code for MAX31855 driver can be found here:

MAX31855 IIO Device Configuration

Device Attributes

The MAX31855 IIO device does not have any device specific attributes.

Device Channels

The MAX IIO device has 0 input channels and 2 output temperature channels.

Temperature channels

The temperature channels are:

  • Channel 0: temp_t
  • Channel 1: temp_i

Each channel has 2 attributes:

  • raw - is the raw temperature value read from the device.
  • scale - is the scale that has to be applied to the raw value in order to obtain the converted real value in degrees Celsius. It has a value of 0.25 for temp_t and 0.0625 for temp_i.
converted_temp [degrees Celsius] = raw * scale

MAX31855 IIO Driver Initialization Example

#define DATA_BUFFER_SIZE 400

struct no_os_spi_init_param spi_param = {
	.max_speed_hz = 100000,
	.mode = NO_OS_SPI_MODE_0,
};

struct max31855_dev *dev;
struct max31855_init_param max31855_param = {
	.spi_init = spi_param
};
struct no_os_spi_desc *spi;

struct max31855_iio_dev *max31855_iio;
struct max31855_iio_dev_init_param max31855_iio_param;
struct iio_data_buffer temp_buffer = {
	.buff = iio_data_buffer,
	.size = DATA_BUFFER_SIZE * 2 * sizeof(int)
};

max31855_iio_param.max31855_dev_init = &max31855_param;
ret = max31855_iio_init(&max31855_iio, &max31855_iio_param);
if (ret)
        return ret;
struct iio_app_device iio_devices[] = {
	{
		.name = "max31855",
		.dev = max31855_iio,
		.dev_descriptor = max31855_iio->iio_dev,
		.read_buff = &temp_buffer,
	}
};

return iio_app_run(iio_devices, NO_OS_ARRAY_SIZE(iio_devices));

For now there is no MAX31855 no-OS demo project.

resources/tools-software/uc-drivers/max31855.1664292149.txt.gz · Last modified: 27 Sep 2022 17:22 by Darius B