Wiki

This version is outdated by a newer approved version.DiffThis version (25 Mar 2024 14:18) was approved by Radu Sabau.

This is an old revision of the document!


MAX22196 No-OS Driver

Supported Devices

Overview

The MAX22194, MAX22196is an industrial octal digital input that translates eight industrial 24V or TTL level inputs to logic level outputs. The device has a serial interface allowing configuration and reading of serialized data through SPI.

GitHub Driver Documentation

Any other driver related documentation can be found on GitHub by following the next link:

Downloads

resources/tools-software/uc-drivers/max22196.1711372542.txt.gz · Last modified: 25 Mar 2024 14:15 by Radu Sabau