This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:max11205 [08 Sep 2022 15:39] – [MAX11205 IIO Device Configuration] Ramona Bolboaca | resources:tools-software:uc-drivers:max11205 [27 Sep 2022 17:22] – fix backlink, moved no-os:overview to no-os Darius B | ||
---|---|---|---|
Line 14: | Line 14: | ||
The goal of ADI Microcontroller No-OS is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. ADI No-OS offers **generic drivers** which can be used as a base for any microcontroller platform and also **example projects** which are using these drivers on various microcontroller platforms. | The goal of ADI Microcontroller No-OS is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. ADI No-OS offers **generic drivers** which can be used as a base for any microcontroller platform and also **example projects** which are using these drivers on various microcontroller platforms. | ||
- | For more information about ADI No-OS and supported microcontroller platforms see: [[: | + | For more information about ADI No-OS and supported microcontroller platforms see: [[: |