Wiki

This version (11 Jul 2023 09:09) was approved by Tinaco Mariel.

LTC6953 - No-OS Driver

Supported Devices

Evaluation Boards

Overview

The LTC6953 is a high performance, ultralow jitter, JESD204B/C clock distribution IC. The LTC6953’s 11 outputs can be configured as up to five JESD204B/C subclass 1 device clock/SYSREF pairs plus one general-purpose output, or simply 11 general-purpose clock outputs for non-JESD204B/C applications. Each output has its own individually programmable frequency divider and output driver. All outputs can also be synchronized and set to precise phase alignment using individual coarse half cycle digital delays and fine analog time delays.

For applications requiring more than 11 total outputs, multiple LTC6953s can be connected together with LTC6952's and LTC6955's using the EZSync or ParallelSync synchronization protocols.

Applications

  • High Performance Data Converter Clocking
  • Wireless Infrastructure
  • Test and Measurement

DC2610A (with LTC6953 on-board chip)

ADI No-OS

The goal of ADI Microcontroller No-OS is to provide reference projects for lower end processors, which can't run Linux or aren't running a specific operating system, and to help those customers using microcontrollers with ADI parts. ADI No-OS offers generic drivers, which can be used as a base for any microcontroller platform and also example projects, which are using these drivers on various microcontroller platforms.

For more information about ADI No-OS and supported microcontroller platforms, visit the No-OS User Guide.

LTC6953 ADI No-OS Driver

Driver Source Code

The source code for the LTC6953 driver can be found here:

The LTC6953 driver also uses the ADI utility library, so make sure you add the necessary files to your project. The source code for the utility library can be found here:

To use the LTC6953 No-OS Driver, you need to provide the specific implementation for the communication APIs as well as the specific data types to be used.

If SPI communication is chosen, these are the three functions to be called by the LTC6953 driver and have to be implemented:

Function Description
no_os_spi_init() initializes the communication peripheral
no_os_spi_write_and_read() writes and reads data to or from the device
no_os_spi_remove() deinitializes the communication peripheral

And these are the two data types that have to be defined:

Function Description
no_os_spi_desc structure holding the SPI descriptor
no_os_spi_init_param structure holding the parameters for SPI initialization

An example of a header file containing the prototypes of the functions which have to be implemented, along with some generic data types they are using, can be found below:

Code Documentation

Source code documentation for the driver is automatically generated using the Doxygen tool and can be accessed in these links:

Device Configuration


Driver Initialization

To use the device, you need to provide the support for the communication protocol (SPI) as mentioned above.

The first API function to be called is ltc6953_init. Make sure that it returns 0, this indicates a successful driver initialization.

Reset Options

To reset the device, you may use below function:

Function Description
ltc6953_reset has the same effect as power-on-reset (POR)

Power Mode Options

To set the power mode of the device, you may use the following functions:

Function Description
ltc6953_power_down_all powers down all output channels
ltc6953_power_down_vco powers down VCO input
ltc6953_power_down sets power mode of a specified channel

Synchronization Settings

To configure the synchronization, you may use the following functions:

Function Description
ltc6953_ezsync_mode EZSync Mode
ltc6953_ssrq_mode Software SYNC or SYSREF request
ltc6953_sync_mode Enable Synchronization

Output Channels Configuration

Each output channel can be configured separately.

Channel Divider

The 11 independent, identical output dividers are driven directly from the input buffer. They divide the input frequency by the output divider value to produce a 50% duty cycle output signal at frequency in 1 of the 11 channels. The function ltc6953_set_output_divider sets the values for the corresponding registers based on the value of the divider.

Channel Delays

Synchronization allows the start times of each output divider to be delayed by the value programmed into the digital delay bits (DDELx). The analog delay blocks (ADELx) are useful in trimming signal timing differences caused by non-ideal PCB routing.

Function Description
ltc6953_set_digital_delay sets digital delay of output channel
ltc6953_set_analog_delay sets analog delay of output channel

Channel SYNC Enable

Enables SYNC or SYSREF on output channel. Use function ltc6953_enable_sync.

Channel SYSREF Mode

Can be configured when output channel's SRQEN bit is set to 1. Use function ltc6953_set_mode.

Mode Description
0 Free Run
1 Gated Pulse
2 Request Pass-Through
3 2*SYSCT Pulses

Channel Output Inversion

The OINV bits of the channel can selectively invert the sense of each output to facilitate board routing without having to cross matched-length traces. Use function ltc6953_invert_output.



Driver Initialization Example

Example Initialization Using Maxim SDK as Platform

#include <stdint.h>
#include <stdlib.h>
#include "ltc6953.h"
 
void main()
{
 
    int ret;
    bool is_ok;
 
    struct max_spi_init_param max_spi_extra = {
	.num_slaves = 1,
	.polarity = SPI_SS_POL_LOW,
	.vssel = MXC_GPIO_VSSEL_VDDIOH,
    };
 
    const struct no_os_spi_init_param ltc6953_spi_ip = {
	.device_id = 1,
	.max_speed_hz = 2000000,
	.chip_select = 0,
	.mode = NO_OS_SPI_MODE_0,
	.bit_order = NO_OS_SPI_BIT_ORDER_MSB_FIRST,
	.platform_ops = &max_spi_ops,
	.extra = &max_spi_extra,
	.parent = NULL,
    };
 
    struct ltc6953_dev *ltc6953_dev;
    struct ltc6953_init_param ltc6953_dev_ip = {
    	.spi_init = ltc6953_spi_ip,
    };
 
    ret = ltc6953_init(&ltc6953_dev, &ltc6953_dev_ip);
    if (ret) 
    	    return ret;
 
    /* Enable VCO Input Filter */
    ret = ltc6953_enable_filter(ltc6953_dev, true);
    if (ret)
    	    return ret;
 
    /* Configure Single Channel */
    uint32_t channel = 0;
 
    /* Set Power Mode for Channel 0 */
    ret = ltc6953_power_mode(ltc6953_dev, channel, 0x00);
    if (ret)
	    return ret;
 
    /* Set Output Divider for Channel 0*/
    ret = ltc6953_set_output_divider(ltc6953_dev, channel, 0x1300);
    if (ret)
            return ret;
 
    /* Read register h00 */
    ret = ltc6953_vco_status(ltc6953_dev, &is_ok);
    if (ret)
	    return ret;
 
    printf("%d", (uint8_t)is_ok);
 
    MXC_Delay(5000);
 
    ret = ltc6953_power_down_all(ltc6953_dev, true);
    if (ret)
    	    return ret;
 
    ret = ltc6953_power_down_vco(ltc6953_dev, true);
    if (ret)
	    return ret;
 
    ret = ltc6953_remove(ltc6953_dev);
    if (ret)
            return ret;
}
resources/tools-software/uc-drivers/ltc6953.txt · Last modified: 11 Jul 2023 07:35 by Joyce Velasco