This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:uc-drivers:ltc2672 [01 Mar 2023 02:50] – minor edits Joyce Velasco | resources:tools-software:uc-drivers:ltc2672 [06 Apr 2023 04:42] (current) – Marc Sosa | ||
---|---|---|---|
Line 44: | Line 44: | ||
To use the LTC2672 No-OS Driver, you need to provide the specific implementation for the communication APIs and the specific types they use. | To use the LTC2672 No-OS Driver, you need to provide the specific implementation for the communication APIs and the specific types they use. | ||
- | If the SPI communication is chosen, there are three functions which are called by the ADXL355 | + | If the SPI communication is chosen, there are three functions which are called by the LTC2672 |
<WRAP center box 60%> | <WRAP center box 60%> | ||
| **no_os_spi_init()** | initializes the communication peripheral. | | | **no_os_spi_init()** | initializes the communication peripheral. | |