Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:uc-drivers:adxl355 [27 Sep 2022 17:23] – fix backlink, moved no-os:overview to no-os Darius Bresources:tools-software:uc-drivers:adxl355 [27 Jun 2023 10:37] (current) – [ADXL355 IIO Code Driver Documentation] Ramona Bolboaca
Line 72: Line 72:
 ==== ADXL355 Code Driver Documentation ==== ==== ADXL355 Code Driver Documentation ====
 Source code documentation for the driver is automatically generated using the Doxygen tool and it is available below: Source code documentation for the driver is automatically generated using the Doxygen tool and it is available below:
-  * [[http://analogdevicesinc.github.io/no-OS/adxl355_8h.html|ADXL355 Header file]] +  * [[http://analogdevicesinc.github.io/no-OS/doxygen/adxl355_8h.html|ADXL355 Header file]] 
-  * [[http://analogdevicesinc.github.io/no-OS/adxl355_8c.html|ADXL355 Source file]]+  * [[http://analogdevicesinc.github.io/no-OS/doxygen/adxl355_8c.html|ADXL355 Source file]]
  
  
Line 204: Line 204:
 ==== ADXL355 IIO Code Driver Documentation ==== ==== ADXL355 IIO Code Driver Documentation ====
 Source code documentation for the IIO driver is automatically generated using the Doxygen tool and it is available below: Source code documentation for the IIO driver is automatically generated using the Doxygen tool and it is available below:
-  * [[http://analogdevicesinc.github.io/no-OS/iio__adxl355_8h.html|ADXL355 IIO Header file]] +  * [[http://analogdevicesinc.github.io/no-OS/doxygen/iio__adxl355_8h.html|ADXL355 IIO Header file]] 
-  * [[http://analogdevicesinc.github.io/no-OS/iio__adxl355_8c.html|ADXL355 IIO Source file]]+  * [[http://analogdevicesinc.github.io/no-OS/doxygen/iio__adxl355_8c.html|ADXL355 IIO Source file]]
 ==== ADXL355 IIO Device Configuration ==== ==== ADXL355 IIO Device Configuration ====
 === Device Attributes === === Device Attributes ===
resources/tools-software/uc-drivers/adxl355.txt · Last modified: 27 Jun 2023 10:37 by Ramona Bolboaca