Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:uc-drivers:ad7091r [13 Nov 2012 15:13] – Modified the table containing the driver's functions. Dan Nechitaresources:tools-software:uc-drivers:ad7091r [05 Jul 2013 10:24] (current) – changed 1 function Lucian Sin
Line 29: Line 29:
 The following functions are implemented in this version of AD7091R driver: The following functions are implemented in this version of AD7091R driver:
 ^ Function       ^ Description     ^ ^ Function       ^ Description     ^
-unsigned char AD7091R_Init(void) | Initializes the SPI communication peripheral. |+| char AD7091R_Init(void) | Initializes the SPI communication peripheral. |
 | void AD7091R_SoftwareReset(void) | Initiate a software reset of the device. | | void AD7091R_SoftwareReset(void) | Initiate a software reset of the device. |
 | unsigned short AD7091R_ReadSample(void) | Initiates one conversion and reads back the result. | | unsigned short AD7091R_ReadSample(void) | Initiates one conversion and reads back the result. |
resources/tools-software/uc-drivers/ad7091r.txt · Last modified: 05 Jul 2013 10:24 by Lucian Sin