This shows you the differences between two versions of the page.
Next revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:ad5758 [25 Apr 2019 10:38] – created Stefan Popa | resources:tools-software:uc-drivers:ad5758 [14 Jan 2021 05:38] – use wiki interwiki links Robin Getz | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
* [[adi> | * [[adi> | ||
+ | |||
+ | ===== Evaluation Boards ===== | ||
+ | * [[adi> | ||
===== Overview ===== | ===== Overview ===== | ||
Line 9: | Line 12: | ||
The device uses a versatile 4-wire serial peripheral interface (SPI) that operates at clock rates of up to 50 MHz and is compatible with standard SPI, QSPI™, MICROWIRE™, | The device uses a versatile 4-wire serial peripheral interface (SPI) that operates at clock rates of up to 50 MHz and is compatible with standard SPI, QSPI™, MICROWIRE™, | ||
- | Applications: | + | ==== Applications |
* Process control | * Process control | ||
* Actuator control | * Actuator control | ||
* PLC and DCS applications | * PLC and DCS applications | ||
* HART network connectivity | * HART network connectivity | ||
+ | |||
+ | ===== HDL Design Description ===== | ||
+ | |||
+ | In the [[: | ||
+ | |||
+ | In order to build the HDL design the user has to go through the following steps: | ||
+ | - Confirm that you have the right tools (the reference design requires Vivado 2018.3) | ||
+ | - Clone the HDL GitHub repository (the project is located at [[https:// | ||
+ | - Build the project (see https:// | ||
+ | |||
+ | ===== Software Setup ===== | ||
+ | |||
+ | In order to perform the software setup the user has to go through the following steps: | ||
+ | - Confirm that you have the right tools (the reference design requires XSDK) | ||
+ | - Clone the No-OS GitHub repository (the project is located at [[https:// | ||
+ | - Follow the instructions provided by [[/ | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
Line 186: | Line 205: | ||
* {{https:// | * {{https:// | ||
* {{https:// | * {{https:// | ||
- | * {{https:// | + | * {{https:// |
* {{https:// | * {{https:// | ||
</ | </ |