Wiki

This version (16 Sep 2020 10:02) was approved by DragosB.The Previously approved version (07 Feb 2020 09:32) is available.Diff

Microcontroller no-OS Drivers

The majority of ADI's products are peripherals to a non-ADI digital engine (FPGA, microprocessor, or microcontroller). While there is major work underway on FPGAs (Xilinx and Altera) and microprocessors (running an operating system like Linux), the efforts on microcontrollers are fragmented due to the diverse nature of the microcontroller market. The goal of these projects (microcontroller/no-OS) is to be able to provide reference projects for lower end processors, which can't run Linux or aren't running a specific operating system, to help customers using microcontrollers with ADI parts.

Drivers List

Accelerometers

Analog to Digital Converters

Analog Front End

Capacitive to Digital & Touch Screen Controllers

D/A Converters (DAC)

Clock Generation Devices

Gyroscopes

Impedance Analyzer

Mobile I/O Expander & Keypad Controller

Multiplexers

Optical

Digital Potentiometers

RF Transceivers

Digital Temperature Sensors

resources/tools-software/uc-drivers-all.txt · Last modified: 13 Feb 2020 12:03 by AndreiD1994