This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:tof-toolbox [08 Jan 2021 22:35] – user interwiki links Robin Getz | resources:tools-software:tof-toolbox [08 Jan 2021 23:23] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
===== Analog Devices Time of Flight Toolbox For MATLAB and Simulink ===== | ===== Analog Devices Time of Flight Toolbox For MATLAB and Simulink ===== | ||
- | ADI maintains a set of tools to model, interface, and target with ADI time of flight devices within MATLAB and Simulink. These are combined into single Toolbox which contains a set of Board Support Packages (BSP). The list of supported boards is provided [[https:// | + | ADI maintains a set of tools to model, interface, and target with ADI time of flight devices within MATLAB and Simulink. These are combined into single Toolbox which contains a set of Board Support Packages (BSP). The list of supported boards is provided [[/ |
==== Quick Start with Toolbox ==== | ==== Quick Start with Toolbox ==== | ||
- | The current stable Toolbox can be downloaded from the [[https:// | + | The current stable Toolbox can be downloaded from the [[https:// |
<WRAP round download> | <WRAP round download> |