Wiki

The most recent version of this page is a draft.DiffThis version (04 May 2022 14:50) was approved by John Joseph.The Previously approved version (09 Nov 2021 06:55) is available.Diff

This is an old revision of the document!


Click here to return back

SigmaStudio+ Shortcuts

Make a Copy of Shape

Select the shape to be copied. Click Alt and drag the shape to create a copy of the shape

Select Multiple Shapes

Individually click on the items to select or click on the left mouse button and drag the cursor over relevant items while holding the Ctrl key

Insert Multiple Connections Between Two Shapes

Press Alt while making a connection between an output pin of the first module to an input pin of the second module. The remaining output pins of the first module will get automatically connected to the remaining input pins of the second module in the same order of the pins

Insert Alias Pin

Press Ctrl and Right Click on an output pin using mouse to insert an Alias pin connected to the output pin

Toggle Control Value

Use Ctrl + T to toggle between the current and previous values of the current control

Module Control Shortcuts

Use Spacebar to toggle the value of checkbox control. Use Up/Down keys to change the value of knob, slider and numeric up-down controls
/srv/wiki.analog.com/data/pages/resources/tools-software/sigmastudiov2/usingsigmastudio/shortcuts.txt · Last modified: 25 Sep 2023 16:54 by Arpit Arora