Click here to return back
Open Existing Project
OpenExistingProject takes in one argument(filePath) and allows the user to open a SigmaStudio+ project in the given filepath. This API returns the SSPResult type.
API
SSPResult OpenExistingProject(string filePath)
Arguments
filePath- The path along with the file name of the project which has to be opened in the SigmaStudio+ application.
Result
SSPResult contains 'IsSuccess' flag and 'Message' information of the OpenExistingProject action.
IsSuccess is 'True' if the project was opened successfully, else 'False'.
Message contains the Success/Failure information in the form of list of string.