Once the module(s) to be used as SigmaStudio+ plugins are configured using the Algorithm Designer, it can be converted into a DLL for redistribution and reuse. Click the 'Build' button from the group of buttons on the top left corner of Algorithm Designer window. The build window will open up and list all the modules in the current Algorithm Designer Project.
The assembly information (details) of the generated DLL can be configured in the 'Assembly Information' section. Following details are supported:
Once the details are entered, click the 'Generate' button to generate the module(s) as a DLL. The Save file dialog that opens up can be used to choose the path and name of the DLL.