Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sigmastudiov2:targetintegration [29 Apr 2022 15:26] – ADSP-21593 and ADSP-SC594 added John Josephresources:tools-software:sigmastudiov2:targetintegration [15 Sep 2023 09:35] (current) Sakthivel Perumal
Line 8: Line 8:
 \\ \\
 ===== Rebuild Demo Application ===== ===== Rebuild Demo Application =====
-The Default Application for ADSP-21489, ADSP-SC573, ADSP-SC584, ADSP-SC589, ADSP-21584, and ADSP-21573, ADSP-21569, ADSP-21593, ADSP-SC594 are supplied with the package. Follow the steps given below to rebuild the Application. The projects can be found under target specific subfolders inside “SigmaStudioPlus-Relx.y.z\Target\Examples\Demo”.+The Default Application for ADSP-21489, ADSP-SC573, ADSP-SC584, ADSP-SC589, ADSP-21584, and ADSP-21573, ADSP-21569, ADSP-21593, ADSP-SC594 and ADSP-SC598 are supplied with the package. Follow the steps given below to rebuild the Application. The projects can be found under target specific subfolders inside “SigmaStudioPlus-Relx.y.z\Target\Examples\Demo”.
  
   - Launch CrossCore Embedded Studio on the SigmaStudio+ Host PC. Specify the workspace when prompted.   - Launch CrossCore Embedded Studio on the SigmaStudio+ Host PC. Specify the workspace when prompted.
-  - Select File->Import. Import SS_App_Core0, SS_App_Core1 and SS_App_Core2 projects into CrossCore Embedded Studio for ADSP-SC573, ADSP-SC584, ADSP-SC589, ADSP-SC589 SAM, ADSP-SC594. +  - Select File->Import->"Existing project into Workspace" option or use "Import an existing CCES project" option in the welcome window. Import SS_App_Core0, SS_App_Core1 and SS_App_Core2 projects of appropriate processor into CrossCore Embedded Studio. In package example projects are available for ADSP-SC573, ADSP-SC584, ADSP-SC589, ADSP-SC589 SAM, ADSP-SC594, ADSP-SC598
-  - Select File->Import. Import SS_App_Core1 and SS_App_Core2 projects into CrossCore Embedded Studio for ADSP-21584, ADSP-21573, ADSP-21593. +  - Select File->Import->"Existing project into Workspace" option or use "Import an existing CCES project" option in the welcome window. Import SS_App_Core1 and SS_App_Core2 projects of appropriate processor into CrossCore Embedded Studio. In package example projects are available for ADSP-21584, ADSP-21573, ADSP-21593. 
-  - Select File->Import. Import SS_App_Core1 project into CrossCore Embedded Studio for ADSP-21489 and ADSP-21569. +  - Select File->Import->"Existing project into Workspace" option or use "Import an existing CCES project" option in the welcome window. Import SS_App_Core1 project into CrossCore Embedded Studio for ADSP-21489 and ADSP-21569. 
-  - Select all the three projects (SS_App_Core0, SS_App_Core1 and SS_App_Core2). Clean and rebuild the projects in the required configuration (Release/Debug) for ADSP-SC573ADSP-SC584, ADSP-SC589 and ADSP-SC594. +  - Select all the core projects of corresponding processor in CCES, Clean and rebuild the projects in the required buildconfiguration (Release/Debug). 
-  - Select the two projects (SS_App_Core1 and SS_App_Core2). Clean and rebuild the projects in the required configuration (Release/Debug) for ADSP-21584, ADSP-21573 and ADSP-21593. +  - The newly generated executable(s) will be present in “Debug” or “Release” folder based on the chosen build configuration, inside the corresponding processor application core projects folder.
-  - Select the project (SS_App_Core1). Clean and rebuild the projects in the required configuration (Release/Debug) for ADSP-21489 and ADSP-21569+
-  - The newly generated executable(s) will be present in “Debug” or “Release” folder based on the chosen configuration.+
 \\ \\
 \\ \\
resources/tools-software/sigmastudiov2/targetintegration.txt · Last modified: 15 Sep 2023 09:35 by Sakthivel Perumal