Wiki

This version (11 Feb 2021 15:08) was approved by Sreesha Y M.

Click here to go back

adi_ss_reset


Prototype

 ADI_SS_RESULT adi_ss_reset( ADI_SS_COMM_HANDLE hSSComm, ADI_SS_COMM_CONFIG *pConf);


Description
The function is to get the reset the SS+ instance to its initial state.

Parameters

Name: phSSn
Type: ADI_SS_SSN_HANDLE *
Direction: Output
Description: Pointer to handle of SS+ instance.

Name: pConf
Type: ADI_SS_COMM_CONFIG *
Direction: Input
Description: Used to pass the configuration parameters to the communication module.


Return value
An appropriate error code of type ADI_SS_RESULT is returned.

resources/tools-software/sigmastudiov2/targetintegration/targetlibapi/apifuncs/adi_ss_reset.txt · Last modified: 25 Jun 2020 07:31 by Sreesha Y M