Wiki

This version (11 Feb 2021 15:08) was approved by Sreesha Y M.

Click here to go back

adi_ss_clearState


Prototype

 ADI_SS_RESULT adi_ss_clearState(ADI_SS_SSN_HANDLE hSSn);


Description
The function is to clear the state memory buffers used by the SS+ instance.

Parameters

Name: hSSn
Type: ADI_SS_SSN_HANDLE 
Direction: Input
Description: Handle to the SSn instance.


Return value
An appropriate error code of type ADI_SS_RESULT is returned.

resources/tools-software/sigmastudiov2/targetintegration/targetlibapi/apifuncs/adi_ss_clearstate.txt · Last modified: 25 Jun 2020 07:50 by Sreesha Y M