This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools-software:sigmastudiov2:targetintegration:targetapplication:mcsupport [29 Jun 2020 07:29] – created Sreesha Y M | resources:tools-software:sigmastudiov2:targetintegration:targetapplication:mcsupport [27 Sep 2023 08:48] (current) – Minor corrections John Joseph | ||
---|---|---|---|
Line 2: | Line 2: | ||
\\ | \\ | ||
=====Microcontroller Mode Support===== | =====Microcontroller Mode Support===== | ||
- | In microcontroller mode, the Target Framework shall process the incoming audio data based on the exported set of code and parameters from SigmaStudio+. The ARM core of ADSP-SC5xx processor acts as a microcontroller, | + | In microcontroller mode, the Target Framework shall process the incoming audio data based on the exported set of code and parameters from SigmaStudio+. The ARM core of ADSP-SC5xx processor acts as a microcontroller, |
\\ | \\ | ||
\\ | \\ | ||
- | A utility is provided with the package | + | A utility is provided with the package |
+ | |||
+ | Please find the steps to export the schematic source files to use with micro controller application: | ||
+ | * Open SigmaStudio+, | ||
+ | * Upon successful compilation of schematic use " | ||
+ | {{: | ||
+ | * Copy the " | ||
+ | * Open Windows Command Prompt and change the working directory to this folder. | ||
+ | * Run the utility as below: | ||
+ | ExportCodeParam.exe < | ||
+ | example:\\ | ||
+ | // | ||
+ | or \\ | ||
+ | // | ||
+ | |||
+ | This generates C source file and header file in the same folder. This utility must | ||
+ | be run multiple times corresponding to the number of schematics within the | ||
+ | core. Use the generated schematic source files to micro controller mode application and rebuild the application.\\ | ||
+ | |||
+ | < | ||
\\ | \\ |