Prototype
ADI_SS_CONNECTION_RESULT adi_ss_connection_Reconfigure( ADI_SS_CONNECTION_HANDLE hSSConnection, ADI_SS_CONNECTION_CONFIG_ITEM eConfigItem, ADI_SS_CONNECTION_CONFIG *pConnectionConfig )
Description
This API reconfigures the connection component based on the chosen config item.
Parameters
Name: eConfigItem Type: ADI_SS_CONNECTION_CONFIG_ITEM Direction: Input Description: Configuration parameter to be reconfigured. Name: pConnectionConfig Type: ADI_SS_CONNECTION_CONFIG* Direction: Input Description: Configuration structure populated by the application. Name: hSSConnection Type: ADI_SS_CONNECTION_HANDLE Direction: Input Description: Handle to the connection component instance.
Return value
An error code of type ADI_SS_COMM_RESULT is returned.
• ADI_SS_COMM_SUCCESS : Communication init successful.
• ADI_SS_CONNECTION_INVALID_CONFIG : Connection Init failed due to invalid config.
• ADI_SS_COMM_FAILED : Communication init failed due to general error.