Wiki

This version (10 Feb 2021 11:02) was approved by Sreesha Y M.

Click here to go back

adi_ss_comm_Parse


Prototype

 ADI_SS_COMM_RESULT adi_ss_comm_Parse(ADI_SS_COMM_HANDLE hSSComm, 
                                      uint32_t nData 
                                     )


Description
This function calls the library parse function to parse a single word from the host.

Parameters

Name: nData
Type: uint32_t
Direction: Input
Description: 32bit received word

Name: hSSComm
Type: ADI_SS_COMM_HANDLE
Direction: Input
Description: Handle to communication component instance.


Return value
An error code of type ADI_SS_COMM_RESULT is returned.
ADI_SS_COMM_SUCCESS : Communication init successful.
ADI_SS_COMM_FAILED : Communication init failed due to general error.

resources/tools-software/sigmastudiov2/targetintegration/commapi/apifuncs/adi_ss_comm_parse.txt · Last modified: 26 Jun 2020 06:24 by Sreesha Y M