Prototype
ADI_SS_COMM_RESULT adi_ss_comm_GetProperties(ADI_SS_COMM_HANDLE hSSComm, ADI_SS_COMM_PROPERTIES *pCommProperties )
Description
API for getting current communication properties.
Parameters
Name: pCommProperties Type: ADI_SS_COMM_PROPERTIES Direction: Input Description: Pointer to structure of type ADI_SS_COMM_PROPERTIES. The fields of this structure is updated by the communication component. Name: hSSComm Type: ADI_SS_COMM_HANDLE Direction: Input Description: Handle to communication component instance.
Return value
An error code of type ADI_SS_COMM_RESULT is returned.
• ADI_SS_COMM_SUCCESS : Communication init successful.
• ADI_SS_COMM_FAILED : Communication init failed due to general error.