Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:sigmastudiov2:modules:sources:sweepswitch [05 May 2021 14:47] Prasad Kamathresources:tools-software:sigmastudiov2:modules:sources:sweepswitch [12 May 2021 12:54] (current) – [Output] Prasad Kamath
Line 7: Line 7:
 \\ \\
 The Sweep block generates a sinewave that sweeps from a start frequency to an end frequency. The sweep rate is determined by the number of sweep steps and cycles per step. In case of the linear sweep, the frequency sweep is linear across time whereas in the case of log sweep input, the frequency sweeps logarithmically cross time. The following variants of the module are available: The Sweep block generates a sinewave that sweeps from a start frequency to an end frequency. The sweep rate is determined by the number of sweep steps and cycles per step. In case of the linear sweep, the frequency sweep is linear across time whereas in the case of log sweep input, the frequency sweeps logarithmically cross time. The following variants of the module are available:
-  * LinearSweepInput +  * Linear Sweep Switch 
-  * LinearSweepWithInputTB +  * Linear Sweep With Switch Tone Burst 
-  * LogSweepInput +  * Log Sweep Switch 
-  * LogSweepWithInputTB+  * Log Sweep With Switch Tone Burst
 \\ \\
 ===== Usage ===== ===== Usage =====
Line 28: Line 28:
 ^Name^ADSP-214xx^ADSP-215xx/ADSP-SC5xx^ADAU145x/1456x^ ^Name^ADSP-214xx^ADSP-215xx/ADSP-SC5xx^ADAU145x/1456x^
 |----------------------------------------|------------------------------------------|--------------------------------------------------|-------------------------------------------| |----------------------------------------|------------------------------------------|--------------------------------------------------|-------------------------------------------|
-|LinearSweep and variants| B & SB & SS+|LinearSweep and variants| Not Supported |Not SupportedSample
-|LogSweep and variants| B & SB & SS|+|LogSweep and variants| Not SupportedNot SupportedSample|
 \\ \\
 ===== Pins ===== ===== Pins =====
 ==== Output ==== ==== Output ====
 ^Name^Type^Description^ ^Name^Type^Description^
-|---------------|-------------------|-----------------------|+|-----------------------------------|-----------------------------------------|-----------------------|
 |Output0|Audio|Output channel 0| |Output0|Audio|Output channel 0|
 \\ \\
Line 47: Line 47:
 \\ \\
 ===== DSP Parameters ===== ===== DSP Parameters =====
-^Parameter Name^Description^ADSP-214xx/SC5xx/215xx^+^Parameter Name^Description^ADAU145x/146x^
 | ----------------------------- | --------------------------------------------------------------------------------------------------- |----------------------------------------------------- | | ----------------------------- | --------------------------------------------------------------------------------------------------- |----------------------------------------------------- |
-|start_freq|normalised value of start frequency|Float+|start_freq|normalised value of start frequency|FixPoint8d24
-|stop_freq|normalised value of end frequency|Float+|stop_freq|normalised value of end frequency|FixPoint8d24
-|numcycles_per_step|Gain, the sinetone wave to be multiplied|Float+|numcycles_per_step|Gain, the sinetone wave to be multiplied|Integer32
-|numsteps|number of steps between start and stop|Float+|numsteps|number of steps between start and stop|Integer32
-|freq_increment| frequency increment defined by range and numsteps |Float+|freq_increment| frequency increment defined by range and numsteps |FixPoint8d24
-|ison |Enabled/Disabled the sweep |Int|+|ison |Enabled/Disabled the sweep |FixPoint8d24|
 \\ \\
 ===== DSP Parameter Computation ===== ===== DSP Parameter Computation =====
resources/tools-software/sigmastudiov2/modules/sources/sweepswitch.txt · Last modified: 12 May 2021 12:54 by Prasad Kamath