Wiki

This version (14 Oct 2021 13:11) was approved by Nikhin Shetty.

Click here to return to the Multiplexers and Demultiplexers page

Solo


Description

If module is enabled, the selected input signal is passed to the selected output channel and rest are muted. In disable state signals get bypassed.

Usage

Select the radio button to route the particular input to output.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
—————————— ——————-- ——————————-- —————————-
Solo B B NA


Pins

Input

Name Type Description
———————————— ————————- ———————————
InputX Audio Input Channel X

Output

Name Type Description
——————————— ————————- ———————————
OutputX Audio Output Channel X

Note:

  • X - Channel Index


Configurable Parameters

GUI Parameter Default Value Range Function Description
—————————————- ———————- —————————— —————————————-
NumChannels 1 1 to 20 Number of input and output channels. Change in this value requires re-compilation
SlewType NoSlew NoSlew/SWSlew Enable or disable SWSlew
StepSize (SWSlew) 10 1 to 24 Step size for transition from one input to other input


DSP Parameters

Parameter Name Description ADSP-214xx/SC5xx/215xx ADAU145x/146x
—————————————- ——————————————————————————-- —————————————- —————————-
StepSize Step size for transition from one input to output Float NA
IsEnable Enable or disable the control Float NA
SelectedIndex Selected channel index Float NA

DSP Parameter Computation

Step = 2^(-1/Step)

resources/tools-software/sigmastudiov2/modules/muxesanddemuxes/solo.txt · Last modified: 14 Oct 2021 13:11 by Nikhin Shetty