This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:tools-software:sigmastudiov2:modules:muxesanddemuxes:simplerouter [05 Feb 2020 06:08] – Added an image Sanjeeva Reddy | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | [[resources/ | ||
+ | ====== Simple Router ====== | ||
+ | \\ | ||
+ | {{: | ||
+ | \\ | ||
+ | {{: | ||
+ | ===== Description ===== | ||
+ | The Simple Router block routes the N different inputs to M different Outputs with multipled by respective gains. | ||
+ | \\ | ||
+ | ===== Usage ===== | ||
+ | Click on the icon to open the Router window to configure the gain for respective input channels for respective outputs. | ||
+ | \\ | ||
+ | ===== Targets Supported ===== | ||
+ | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | ||
+ | |Simple Router| No | Yes|No| Yes| | ||
+ | \\ | ||
+ | ===== Pins ===== | ||
+ | ==== Input ==== | ||
+ | ^Name^Type^Description^ | ||
+ | |Input0|Audio|Input channel 0| | ||
+ | |Input1|Audio|Input channel 1| | ||
+ | ==== Output ==== | ||
+ | ^Name^Type^Description^ | ||
+ | |Output0|Control|Output channel 0| | ||
+ | \\ | ||
+ | ===== Configurable Parameters ===== | ||
+ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | |SlectedInputTab< | ||
+ | |GainDB_Output< | ||
+ | |ISDb_Output< | ||
+ | |NumInputs|2|20|Number of input channels. Change in input channels requires re-compilation| | ||
+ | |NumOutputs|1|20|Number of input channels. Change in output channels requires re-compilation| | ||
+ | \\ | ||
+ | ===== DSP Parameters ===== | ||
+ | ^Parameter Name^Description^ADSP-214xx/ | ||
+ | |GainArray|scaling of the inputs|Float| | ||
+ | |OutputArray|scaling of the inputs|Float| | ||
+ | \\ | ||