This shows you the differences between two versions of the page.
Previous revisionLast revision | |||
— | resources:tools-software:sigmastudiov2:modules:muxesanddemuxes:indexselectablemultiplexer [15 Jan 2021 06:04] – [Variants] Nikhin Shetty | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | [[resources/ | ||
+ | ====== Index Selectable Mux ====== | ||
+ | {{: | ||
+ | \\ | ||
+ | {{: | ||
+ | \\ | ||
+ | {{: | ||
+ | ===== Description ===== | ||
+ | The Index Selectable Mux block routes one(Mono) or two(Stero) of the inputs to output, based on the control input index value from the Index Lookup Table, RMS Table or DC Input. | ||
+ | |||
+ | Index Selectable Mux (Stereo - SW Slew) block allows smooth transition when switching inputs. | ||
+ | \\ | ||
+ | ===== Variants ===== | ||
+ | - Index Selectable Mux (Mono - No Slew) | ||
+ | - Index Selectable Mux (Stereo - No Slew) | ||
+ | - Index Selectable Mux (Stereo - SW Slew) | ||
+ | \\ | ||
+ | ===== Targets Supported ===== | ||
+ | ^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/ | ||
+ | |Index Selectable Mux (Mono - No Slew)| Yes | Yes|Yes| Yes| | ||
+ | |Index Selectable Mux (Stereo - No Slew)| Yes | Yes|Yes| Yes| | ||
+ | |Index Selectable Mux (Stereo - SW Slew)| No | Yes|No| Yes| | ||
+ | \\ | ||
+ | ===== Pins ===== | ||
+ | ==== Input ==== | ||
+ | ^Name^Type^Description^ | ||
+ | |Index|Control|Controls the routing of inputs to the output channel| | ||
+ | |Input0|Audio|Input Channel 0| | ||
+ | |Input1|Audio|Input Channel 1| | ||
+ | |Input2|Audio|Input Channel 2(only for stereo)| | ||
+ | |Input3|Audio|Input Channel 3(only for stereo)| | ||
+ | ==== Output ==== | ||
+ | ^Name^Type^Description^ | ||
+ | |Output0|Audio|Output channel 0| | ||
+ | |Output1|Audio|Output channel 1(only for stereo)| | ||
+ | \\ | ||
+ | ===== Configurable Parameters ===== | ||
+ | ^GUI Parameter Name^Default Value^Range^Function Description^ | ||
+ | |StepSize|0|-10 to 10|Controls the rate changing from one input to other input(only for SW Slew)| | ||
+ | |NumChannels|2|2 to 20 |Number of input channels. Change in this value requires re-compilation(only for mono)| | ||
+ | |NumChannels_Stereo|4|4 to 20 |Number of input channels. Change in this value requires re-compilation(only for stereo)| | ||
+ | \\ | ||
+ | ===== DSP Parameters ===== | ||
+ | ^Parameter Name^Description^ADSP-214xx/ | ||
+ | |StepSize|Controls the rate changing from one input to other input|Float| | ||
+ | \\ |