This is an old revision of the document!
Click here to return to the Mixers and Splitters page
The NxM Mixer block multiplies the inputs with respective gains and mixes N number of inputs and sends the result to the M number of outputs.
Click on the icon to open the NxM Mixer window to configure the gain for respective input channels for respective outputs.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
NXMMixer | No | Yes | No | Yes |
Name | Type | Description |
---|---|---|
Input0 | Audio | Input channel 0 |
Input1 | Audio | Input channel 1 |
Name | Type | Description |
---|---|---|
Output0 | Control | Output channel 0 |
GUI Parameter Name | Default Value | Range | Function Description |
---|---|---|---|
GainDB_OutputM_InputN | 0 dB | -30 to 6 dB | Gain factor |
ISDb_OutputM_InputN | True | True/False | Decides the Gain control in db/linear |
NumInputs | 2 | 20 | Number of input channels. Change in this value requires re-compilation |
NumOutputs | 1 | 20 | Number of output channels. Change in this value requires re-compilation |
Parameter Name | Description | ADSP-214xx/SC5xx/215xx |
---|---|---|
GainArray | scaling of the inputs | Float |