Wiki

This version (18 Oct 2021 06:30) was approved by Nikhin Shetty.

Click here to return to the Mixers and Splitters page

Balance Fader Generic



Description


Reposition the image in front of the listener by adjusting gain levels of speakers. User can configure all the front and rear channel coefficients values.

Usage

Click on the config button to open the balance fader coefficient window to configure the gain for respective input channels for respective outputs.

Targets Supported

Name ADSP-214xx ADSP-215xx/SC5xx ADAU145x/146x
—————————— ——————-- ——————————-- —————————-
Balance Fader B B NA


Pins

Input

NameTypeDescription
————————————-——————-——————————————-
FrontRight_InputAudioFront right channel input to the balance fader
FrontLeft_InputAudioFront left channel input to the balance fader
RearRight_InputAudioRear right channel input to the balance fader
RearLeft_InputAudioRear left channel input to the balance fader
Center_InputAudioCenter channel input to the balance fader
SW_InputAudioSub woofer input to the balance fader

Output

NameTypeDescription
————————————-——————-——————————————-
FrontRight_OutputAudioFront right channel output from the balance fader
FrontLeft_OutputAudioFront left channel output from the balance fader
RearRight_OutputAudioRear right channel output from the balance fader
RearLeft_OutputAudioRear left channel output from the balance fader
Center_OutputAudioCenter channel output from the balance fader
SW_OutputAudioSub woofer output from the balance fader


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
————————————-——————————-———————————————————————-
Balance0 -10 to 10Controls the balance of audio level between the left and right channels
Fade0-10 to 10Controls the fade out of audio level between the front and rear channels.
StepSize (SW Slew)118 to 16Controls the smooth transition of change in audio level
Config NA NA Adjust the gain level of each parameter value of Balance and Fader configuration


DSP Parameters

Parameter Name Description ADSP-214xx/SC5xx/215xx ADAU145x/146x
—————————————- ——————————————————————————-- —————————————- —————————-
BalanceBalance of audio level between the left and right channelsFloat NA
FadeFade out of audio level between the front and rear channelsFloat NA
StepSizeAllows smooth transition of change in audio levelFloat NA
BFrontRight Balance Front Right channel coefficients Float NA
BFrontLeft Balance Front Left channel coefficients Float NA
BRearRight Balance Rear Right channel coefficients Float NA
BRearLeft Balance Rear Left channel coefficients Float NA
BCenter Balance Center channel coefficients Float NA
BSubWoofer Balance Subwoofer channel coefficients Float NA
FFrontRight Fader Front Right channel coefficients Float NA
FFrontLeft Fader Front Left channel coefficients Float NA
FRearRight Fader Rear Right channel coefficients Float NA
FRearLeft Fader Rear Left channel coefficients Float NA
FCenter Fader Center channel coefficients Float NA
FSubWoofer Fader Subwoofer channel coefficients Float NA


resources/tools-software/sigmastudiov2/modules/mixersandsplitters/balancefadegeneric.txt · Last modified: 18 Oct 2021 06:12 by Nikhin Shetty