Wiki

This version (11 May 2021 16:00) was approved by Prasad Kamath.The Previously approved version (19 Mar 2021 02:04) is available.Diff

Click here to return to the Master Control Port page

Master Control Port Status



Description


The master control port Status block sends out the Master control port status in the output pins. Master control errors can be cleared by setting input pin to non-zero value

Usage


Use the output pins to monitor master control port status and error. The error can be cleared by inputting a non-zero value at the input.

Targets Supported

NameADSP-214xxADSP-215xx/ADSP-SC5xxADAU145x/1456x
—————————————-——————————————————————————————--——————————————-
Master Control Port Status Not Supported Not Supported Sample


Pins


Input Pins

NameTypeDescription
—————————————————————————————--
ClearErrorsControlAny non -zero value in the input clears the error.


Output Pins

NameTypeDescription
———————————————————-————————————--
StatusControlOutputs 1 while the Master control port is busy, otherwise outputs 0
I2CErrorStatusControlIt is a 2 bit value. Bit-0 is set if I2C error is encountered. Bit-1 is set when timeout error occurred.


Configurable Parameters


Not applicable

DSP Parameters


Not applicable

DSP Parameter Computation


Not applicable

resources/tools-software/sigmastudiov2/modules/mastercontrolport/mastercontrolportstatus.txt · Last modified: 11 May 2021 16:00 by Prasad Kamath