This is an old revision of the document!
Click here to return to the Master Control Port page
There are two different versions of I2C Read module.
The 'I2C Periodic Read' block reads a particular sub address from any I2C slave periodically and sends the value read in the output pin.
The 'I2C Read with external Trigger' block reads a particular sub address from any I2C slave when a rising edge is detected in the input pin.
Click on the configure button to configure the parameters for I2C read.
Create Multiple instances for monitoring multiple slaves/ multiple sub address from same slave.
Name | ADSP-214xx | ADSP-215xx/ADSP-SC5xx | ADAU145x/1456x |
---|---|---|---|
—————————————- | —————————————— | ————————————————-- | ——————————————- |
I2C Read | Not Supported | Not Supported | Sample |
Name | Type | Description |
---|---|---|
————— | ——————- | ———————-- |
Trigger | Control | Rising edge in this signal initiates read. |
Name | Type | Description |
---|---|---|
————— | ——————- | ———————-- |
OutputX | Control | Outputs data read over I2C |
GUI Control Name | Default Value | Range | Function Description |
---|---|---|---|
—————————————————- | ———————- | —————————————— | ———————————————————————- |
I2CBitrate | 400 kHz | 20 - 400 kHz | I2C Speed |
I2CDeviceAddress | 0 | 0 – 127 | I2C Slave Device Address |
I2CDeviceAddressBits | 8-Bit | 8-Bit/7-Bit | 7 or 8 bit i2c address |
I2CDeviceAddressFormat | Hex | Hex/Dec | Address format |
DataLength | 4 | 1-4 | Length of the data to be read |
SubAddressBytes | 2 | 1-4 | Length of the sub address |
ReadAddress_OutputX | 0 | 0 to Pow(2, Address Length) - 1 | Sub- address of the slave to be read |
InitialOutputValue_OutputX | 0 | -2147483648 to 2147483647 | Value in the output pin till the first read is complete. |
Note: X indicates the channel number
Not applicable
Not applicable