Wiki

This version (18 May 2021 09:01) was approved by John Joseph.The Previously approved version (07 May 2021 15:02) is available.Diff

Click here to return to the IO page

SPDIF Output



Description


The SPDIF Output blocks route signals between the schematic design and the hardware's SPDIF pins.

Usage


Use the output block's drop-down list control to select from the available SPDIF outputs.

Note: These blocks are only available for use with DSPs that have SPDIF I/O.



Targets Supported

NameADSP-214xxADSP-215xx/ADSP-SC5xxADAU145x/1456x
—————————————-——————————————————————————————--——————————————-
SPDIF Output Not supported Not supported Sample


Pins

Input

NameTypeDescription
—————————-——————————————————--
Output Audio Interface read output channel


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
—————————————- ———————- ————————————- —————————————-
SelectedSPDIFOPChannel00 to 2 Selects the SPDIF out channel


DSP Parameters

Not applicable


DSP Parameter Computation

Not applicable

resources/tools-software/sigmastudiov2/modules/inputoutput/spdifoutput.txt · Last modified: 12 May 2021 13:44 by Prasad Kamath