Click here to return to the IO page
The Output block routes signals to the hardware's physical outputs. Each block is linked to a single output channel.
Using the drop-down list, select the output channel to associate with a particular block.
Observe that as you drag more output blocks to your schematic, the number of output channels available in the drop-down list decreases because each output can only be associate with a single output block at a time.
The hardware outputs for a particular processor are limited. While designing you can see the number of outputs that are still available from the HWOutputs item of the Resources window.
Name | ADSP-214xx(Sample) | ADSP-214xx(Block) | ADSP-215xx/ADSP-SC5xx(Sample) | ADSP-215xx/ADSP-SC5xx(Block) |
---|---|---|---|---|
Output | Yes | Yes | Yes | Yes |
Name | Type | Description |
---|---|---|
input0 | Audio | Outputs the audio to the hardware pin |
GUI Parameter Name | Default Value | Range | Function Description |
---|
No DSP Parameters