This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudiov2:modules:inputoutput:interfacereadio [12 May 2021 13:39] – [Output] Prasad Kamath | resources:tools-software:sigmastudiov2:modules:inputoutput:interfacereadio [12 May 2021 13:40] (current) – [Description] Prasad Kamath | ||
---|---|---|---|
Line 9: | Line 9: | ||
Interface Read module will keep giving the parameter read from the EEPROM during self boot as output. When the current parameter is changed during execution, the Interface write module updates the present value in the Interface read block.The Interface read module will always have the current parameter setting.\\ | Interface Read module will keep giving the parameter read from the EEPROM during self boot as output. When the current parameter is changed during execution, the Interface write module updates the present value in the Interface read block.The Interface read module will always have the current parameter setting.\\ | ||
+ | \\ | ||
NOTE: \\ | NOTE: \\ | ||
- | | + | Make sure that the interface read and interface write modules that are with each interacting have the same Interface number paramter.\\ |
\\ | \\ |